Part Number: LM5119 Tool/software: I am looking for a Multiphase Buck controller that will handle the -55C to +125C temperature range.
I have used the LM5119 in the past but the temp range is only -40C to +85C. In addition to the extended temp range…
Part Number: LM5119 Other Parts Discussed in Thread: PMP30464 , , LM5149 Tool/software: Hi Team,
This is Gree FAE Ryker. Recently Gree wants to find a high-power BUCK as below request. I have promoted LM5119 and reference design PMP30464 firstly. But…
Part Number: LM5119 Hi!
I have recently finished a schematic for a LM5119 Dual Output design. I was hoping to have it reviewed to see if any parts of the design need to be changed. Attached is the schematic. I used the LM(2)5119 Calculator to get…
Part Number: LM5119 Tool/software: Hi TI expert
I found the application report ZHCA658 from TI website to study the RC snubber circuit design.
In the section 1.3, it gives the formula of the equivalent circuit[figure 3], and the selection guide of…
Part Number: LM5119 Other Parts Discussed in Thread: PMP10260 , PMP20818 , CSD18534Q5A Hi,
It is said that Synchronous Buck "Freewheel" FETs must have Qgd/Qgs <1?
As such, please advise why ti.com has two reference designs of synch bucks, which violate…
Part Number: LM5119 I recently got an LM5119 evaluation board and have been happy with the performance so far. I have an application that would require two 40V, 10A outputs and this part seems like a perfect fit. However, one thing I have noticed in the…
Part Number: LM5119 Hi, TI expert.
The customer has an inquiry about UVLO operation of LM5119.
- Condition : When forced UVLO off, UVLO off after 321ms Delay by external circuit.
- Questions)
Low Side FET operates intermittently under the condition…
Hi Colin,
Both of the below two methods works. I would prefer to use method 2 because no external amplifier is required.
1. Use external error amplifier. The output of external error amplifier is connected to COMP pins of all LM5119.
2. Use the…
Part Number: LM5119 Hi,
my assigned customer wants to use LM5119 in this configuration:
dual phase, Vin = 18V..60V, Vout = 12V, I_load_cont = 12A, I_peak = 16A
They tested the EVM and noticed, that the current in both phases differs a lot. Measuered…