Other Parts Discussed in Thread: LM5119Q , LM5119 Dear Specialist.
Our customer is considering to replace from LTC3890 to LM5119Q. They intend to design 4 phase interleave using 2 ICs. They shared each output of error amp to be same duty cycles in each phase…
Other Parts Discussed in Thread: LM5119 Hi Ti Team,
We are using the LM5119 dual synchronous Buck converter for our application which require 3.3V of 3A and 5V of 4A output , For this we are going with typical Application Schematic given in LM5119 Datasheet…
Other Parts Discussed in Thread: LM5119 , LM5119EVAL Good day,
Firstly, thank you very much for your webbench software.
I ran a design on Webbench with the LM5119. When I export the CAD files, I see that only a schematic is available. Is a PCB layout available…
Other Parts Discussed in Thread: LM5119 , UCC27211 , LM5116 Got the below question:
I'm using TI UCC27211 driver to drive the buck MOSFETs and I want to make sure I'm connecting the LM5119 correctly. In order to drive the high side input of the UCC27211…
Other Parts Discussed in Thread: LM5119 i am trying to design a dc-dc converter, and i was going to use lm5119 with its high output current and dual channels,
however if i increase my ambient temperature in webench designing tool to 50, it uses both channels…
Other Parts Discussed in Thread: LM5117 , LM5119 Dear, All
There are the following descriptions in P16 'HO and LO Output Drivers' of the data sheet. "The LO and HO outputs are controlled with an adaptive dead-time methodology which insures that both…
Other Parts Discussed in Thread: LM5117 , LM5119 Dear, All
Voltage Maximum Ratings of SW Pin is short in the circuit of the customer. Therefore it is considered whether they connect the signathey which I pushed for resistance to input of SW Pin. There is…
Other Parts Discussed in Thread: LM5119 , LM5116 Hello,
Can the LM5119 be used as a constant-current battery charger (operate continuously in current limit mode) if hiccup limiting is disabled? A client has a mixed-load application that would occasionally…
Other Parts Discussed in Thread: LM5119 , LM119 We have an application for an interleaved-output LM5119 based on the PMP7819 reference design. The output current levels and types of loads will vary greatly, including powering up into (and/or, being connected…
Other Parts Discussed in Thread: LM5119 , LM5116 We have an application for a 16V-60Vin, 14Vout @ 1A-30A regulator.
The 400W 33V-60Vin 12Vout reference design for the LM5119, PMP7819, looks good but we'd like to lower the Vin-min value to 19V or less, preferably…