Part Number: LM5122-Q1 Hi Team,
is there design calculator and schematic review guidance for LM5122-Q1? Thanks.
there is webench design and I want to see if there is excel calculator.
BRs
Given
Part Number: LM5122-Q1 Other Parts Discussed in Thread: LM5122 , LM25122-Q1 Can LM5122-Q1 provide load carrying capacity greater than 400W at 20-25V output?
If not, compared with LTC3787, it can provide load capacity greater than 400 at 20-25v output…
Part Number: LM5122-Q1 Other Parts Discussed in Thread: LM5122 We currently have a multi-phase boost using two LM5122. The circuit will boost the input voltage of 9-48V to 48V.
This works perfectly and no issues thus far.
Our customer requirements have…
Part Number: LM5122-Q1 Other Parts Discussed in Thread: LM5122 Hi, TI expert.
I have a question about the LM5122-Q1.
Q1) I want to use LM5122-Q1 as output 100V. Is there any solution or data designed with output 100V?
Q2) Can LM5122-Q1 be used for…
Part Number: LM5122-Q1 Other Parts Discussed in Thread: LM5122 Dear Sir/ Madam,
Greetings of the Day!
We are using the LM 5122-Q1 Asynchronous Boost converter in master slave (Two-Converters) Configuration for our application. The input Voltage is 28V…
Part Number: LM5122-Q1 Hi Expert, When customer is using the LM5122+CSD19532Q5B scheme to boost the voltage, VIN=12V, VOUT=70V, Fsw=110Khz, and it can work normally with a 100R load; when the load resistance drops to 70R, the output voltage is pulled down…
Part Number: LM5122-Q1 Other Parts Discussed in Thread: LM5122 , LM5170 Hi
I would like to design multi phase boost application, here is design requirement,
The boost input voltage is 4.2V~9.6V and output is 12.3V/62A. may I use the LM5122 that configuration…
Part Number: LM5122-Q1 Other Parts Discussed in Thread: LM5123-Q1 Hi team,
I'd like to choose a boost controller that can support 360W output, Vin is 14.4V.
Can LM5122-Q1 can meet the requirement?
Or what device to you recommend in this case?
Thank…
Part Number: LM5122-Q1 Other Parts Discussed in Thread: LM5122 , LM5156 , Hi, I have a question about the topology of the Synchronous Boost Controller. I was wondering why there is a mosfet instead of the typical fast recovery diode before the load.
We would…
Part Number: LM5122-Q1 Other Parts Discussed in Thread: LM5122 Hi team, Good day.
Based on the LM5122-Q1 datasheet, the open-loop response transfer function is defined as,
Our customer have three questions regarding this transfer function:
1. Is this…