Part Number: LM5123-Q1 Other Parts Discussed in Thread: LM5122 , LM5170 Hi team,
I plan to design >>400W boost regulator using LM5123-Q1.
I found LM5123-Q1 Boost Controller Qucickstart Design Tool on TI.com, but it only seems to support <100W.…
Part Number: LM5123-Q1 Other Parts Discussed in Thread: LM5155
Hi team,
I have questions about LM5123-Q1 when it is configured with TAS5828 Class-H audio amp. Please refer to below customer's configuration.
---
Customer’s Battery spec: 13V(discharged…
Part Number: LM5123-Q1 Other Parts Discussed in Thread: LM5122
Hi,
I would like to get 24V 10A (in pick) on output from single LiFePo cell (3,6V).
Does it work with selected element? I will supply the electric bike (and not only, thats why I would like…
Part Number: TAS6584-Q1 Other Parts Discussed in Thread: LM5123-Q1 Tool/software: I am testing using TAS6584-Q1 2ea and LM5123-Q1.
Audio input uses TDM and output channels use 4 channels each, for a total of 8Ch.
Even if no signal is input to Audio Input…
Part Number: LM5123-Q1 Dear Forum,
I am designing a boost converter using the LM5123-Q1. The input voltage range is 10V to 26V. The output voltage must be 28V with an output current from 0 to 3.3A (92W max). With the help of Webench, I have created the…
Part Number: LM5123-Q1 Dear teams,
My customer is using LM5123. Due to the maximum voltage limit, customer is thinking about following solution: They want to add a PMOS on the red arrow point, then add a comparator before the PMOS to control. Once the…
Part Number: LM5123-Q1 Hi
Could you help suggest to use at input voltage 8V ~13V to 15V 10A , Boost ic
Is LM5123 ok or have other suggestions
Thanks you
Part Number: LM5123-Q1-DESIGNCALC Hello!
I've encountered two differences between the design tool an the datasheet:
The datasheet mentions 470 p F for C_VREF (Section 8.3.7), the picture in the design tool states 470 n F.
Using an V_UVLO_ON of 8 V,…