Part Number: LM5137 Hi TI team,
for programable variable output what will be the safe operating minimum and maximum duty cycle for LM5137
Input voltage- 48Vdc
Variabale output voltage- 1V to 24V
Power - 150W (max with auto ranging)
Current-…
Part Number: LM5137 Hi,
We consider to use LM5137 for the DC/DC design, and the input voltage is about 41V to 63V(15 string ternary
lithium iron battery), the output is about 48V/20A;
Now, we need the output voltage is 48V when the input voltage…
Part Number: LM5137-Q1 When using the LM5137-Q1 in interleaved, or in multiphase, operation, is it required to connect all of the EN1/2 pins?
In that case, the hysteresis current sources will probably all add up and lead to an increased hysteresis,…
Part Number: LM5137-Q1 Other Parts Discussed in Thread: LMG708B0 Hi, could you please help check my schematic for the LM5137-Q1 to see if there are any issues?
The circuit diagram is attached below.
I selected Infineon MOSFETs for this design. The…
Part Number: LM5137 Other Parts Discussed in Thread: LMG5200 , LMG2100R044 , Hi, Teams
I plan to use the LM5137 to design the buck converter with 24V/15A and 5V/6A dual output and I will use our GaN LMG2100R044 and LMG5200 in each power rail. But our…
Part Number: LM5137-LM25137-DESIGN-CALC Other Parts Discussed in Thread: LM5137 Hi TI team,
I'm considering to use the LM5137 to configure as the inverting buck-boost controller? Is that OK from the technical side? and Is there any calculation to configure…
Part Number: LM5137-Q1 Other Parts Discussed in Thread: LM5137F-Q1 Dear TI experts,
My customer now tests their own PCB which include LM5137-Q1. But still output is not detected.
They made the schematic just as same as Figure 8-20 in the datasheet…
Part Number: LM5137 Hi Teams,
My customer is designing the power board for the robot board, which is powered by a 48V battery with 48V input and 48V output 24V@20A The attachment is a schematic diagram, please help review it.
Thank you!
LM5137_2026…
Part Number: LM5137-LM25137-DESIGN-CALC Other Parts Discussed in Thread: LM5137F-Q1 , LM5137-Q1 Hello
please provide PSpice model of the LM5137-Q1, LM5137F-Q1 ASAP.
thanks
Part Number: LM5137-Q1 Hi
We are currently using the LM5137-Q1 to implement a four-phase synchronous buck converter.
The system specifications are as follows:
Input voltage range: 30–50V
Output voltage range: 9–15V
Maximum load current: 70A…