Part Number: LM5137-LM25137-DESIGN-CALC Other Parts Discussed in Thread: LM5137F-Q1 , LM5137-Q1 Hello
please provide PSpice model of the LM5137-Q1, LM5137F-Q1 ASAP.
thanks
Part Number: LM5137-LM25137-DESIGN-CALC Other Parts Discussed in Thread: LM5137-Q1 Hi there,
I just wanted to check if there has been any progress on releasing a PSPICE model for the LM5137-Q1 for simulation purposes?
In a previous E2E thread it was…
Part Number: LM5137-LM25137-DESIGN-CALC Other Parts Discussed in Thread: LM5137 Hi TI team,
I'm considering to use the LM5137 to configure as the inverting buck-boost controller? Is that OK from the technical side? and Is there any calculation to configure…
Part Number: LM5137-LM25137-DESIGN-CALC Other Parts Discussed in Thread: LM5137 Hi team,
I'm using the LM5137 to evaluate a solution, and I want to configure LM5137 with the two phase invertin buck-boost controller topology, is there any desig tool…
Part Number: LM5137-Q1 Other Parts Discussed in Thread: LM5137F-Q1-EVM12V , PMP41158 Hi
We are designing a 4-phase synchronous BUCK using the LM5137-Q1 . System conditions are:
Input voltage: 48 V
Output voltage: 14.5 V
Maximum output current…
Part Number: TPSM63610-DESIGN-CALC Other Parts Discussed in Thread: TPSM5D1806 Dear TI Team,
I want to generate 3.3V & 2.5V from 6V by using the power module TPSM5D1806MRDBR-ET. But this part is not available in the TI simulation tool (web bench & Tina…
Part Number: LM25139-DESIGN-CALC Other Parts Discussed in Thread: LM25139-Q1EVM-440 The schematic has ISENSE pin connected after the shunt, and VOUT pin connected between inductor and shunt. According to the datasheet and the schematic for the evaluation…