Part Number: LM5137-Q1 Other Parts Discussed in Thread: LMG708B0 Hi, could you please help check my schematic for the LM5137-Q1 to see if there are any issues?
The circuit diagram is attached below.
I selected Infineon MOSFETs for this design. The…
Part Number: LM5137-LM25137-DESIGN-CALC Other Parts Discussed in Thread: LM5137F-Q1 , LM5137-Q1 Hello
please provide PSpice model of the LM5137-Q1, LM5137F-Q1 ASAP.
thanks
Part Number: LM5137-Q1 Other Parts Discussed in Thread: LM5137F-Q1 Dear TI experts,
My customer now tests their own PCB which include LM5137-Q1. But still output is not detected.
They made the schematic just as same as Figure 8-20 in the datasheet…
Part Number: LM5137-Q1 When using the LM5137-Q1 in interleaved, or in multiphase, operation, is it required to connect all of the EN1/2 pins?
In that case, the hysteresis current sources will probably all add up and lead to an increased hysteresis,…
Part Number: LM5137-Q1 Hi
We are currently using the LM5137-Q1 to implement a four-phase synchronous buck converter.
The system specifications are as follows:
Input voltage range: 30–50V
Output voltage range: 9–15V
Maximum load current: 70A…
Hi Yuming,
Nice to hear from you again. The LM5137-Q1 is somewhat difference in terms of the FB voltage, error amp gm, CS amp gain, etc. Use the quickstart calculator to derive compensation values (making sure to derate ceramic Cout when doing so…
Part Number: LM5137-Q1 Other Parts Discussed in Thread: LM5137F-Q1-EVM12V , PMP41158 Hi
We are designing a 4-phase synchronous BUCK using the LM5137-Q1 . System conditions are:
Input voltage: 48 V
Output voltage: 14.5 V
Maximum output current…
Part Number: LM5137-Q1 Other Parts Discussed in Thread: LM5137F-Q1-EVM12V Is it possible to modify the LM5137F-Q1-EVM12V evaluation board to provide 24V/40A output from a 45V input? If so, what changes need to be made?
Part Number: LM5137-Q1 Dear TI experts,
My customer made their schematic using LM5137-Q1. Could you review it?
LM5137-Q1_Power block(DCDC).pdf
Best regards,
Chase