Part Number: LM5141-Q1 Tool/software: HI,
We are using LM5141-Q1 in one of our projects and designed to generate 12V .When we turn on the board at start it generates 5V instead of 12V. But when ECU is restarted meaning hard reset is applied it generates…
Part Number: LM5141-Q1 Tool/software: Hello,
I wanted to run a LTSpice simulation, but the model is only available for PSpice. Is it possible to get a version, I can include in LTSpice (my university preferes LTSPice).
Thank you.
Best regards
Part Number: LM5141-Q1
I came across this IStep (transient step load current) which is 4A. is IStep assumed value or is there any caluclation involved to get this value as 4Amp.
if any calculations involved please let me know.
Thank you.
Part Number: LM5141-Q1 Other Parts Discussed in Thread: LM5145 , LM61440-Q1 , LM63460-Q1 , 1.Is there any reference circuit with DCR current sensing method-In WEBBENCH tool only current sense method is given
2.How to select HS & LS Mosfet ?-From datasheet…
Part Number: LM5141-Q1 Hello team,
I'd like to use LM5141-Q1 to design a single BUCK with:
Vin: 4V~36V
Vout: 3.3V
Iout: 14A
I understand that t he output current is determined by the power stage componnets (MOSFET and inductor), not the…
Part Number: LM5141-Q1 Tool/software: Hello Team,
We are using the LM5141-Q1 in our design for converting 12V input to 3.3V @ 10A output. The schematic is attached below. Kindly request your expert review and comments on the implementation. Key Specs…
Part Number: LM5141-Q1 Hi team,
I want to use WeBench to simulate load transient response for LM5141-Q1. But the simulation failed as shown below
How can I fix this?
Regards,
Bengi Long
Part Number: LM5141-Q1 Other Parts Discussed in Thread: LM5141 , LM25143-Q1 , , LM5143A-Q1 , LM25148-Q1 , LM5148-Q1 , LM25141-Q1 , LM25149 Hello team,
I found the max current LM5141 can support is 30A in the Data sheet , but I have question w.r.t the…
Part Number: LM5141-Q1 I have a question about inductor selection for LM5141-Q. I checked the required inductor value using two different ways. But I got different results. I am little confused. I would like to know which is correct way to determine the…
Part Number: LM5141-Q1 Hi,
can you tell me the difference between Automotive and industrial part for LM1541.We designed for 12V output (Automotive part) output is not coming. output is coming with industrial part.