Part Number: LM5143 Tool/software: Dear Friends,
as the title, I wonder the LM5143 whether need calculate the sunnber circuit analyze?
I'm looking forward replying.
Thanks
Part Number: LM5143 Tool/software: Hi,
I'm using LM51343 for converter (9V to 12Vin, Vout1- 8.5V at 5A and Vout2 - 5V at 5A). At 12Vin my converter was working fine.
But 10.5Vin my 5V output starts to oscillate at 1Khz to 5Khz. So I suspected it was…
Part Number: LM5143 Tool/software: Hi,
Please kindly review our LM5143 schematic diagram, our input voltage is 19-24V,+/-10%, and output 12V/25A, the max. output power is 300W, thanks. LM5143_19-24V_IN_12V_25A_OUT_300W.pdf
Part Number: LM5143 Tool/software: Hi,
We use LM5143 for charger to Battery.My application as below:
32V input,18V to 25V output,single output,two-phase synchronous buck.We want to output 11Amps.
1 - Can this be achieved?
2 - How to calculate…
Part Number: LM5143-Q1 Other Parts Discussed in Thread: LM5143 , LM5170 Tool/software: I am using LM5143 in IBB configuration like the diagram below. Would the controller be able to support current flow in the opposite direction? The customer is curious…
Part Number: LM5143 Tool/software: Hi,
I'm going to use LM5143 to generate single output (10Vin to 3.3V @ 30A). Is this buck controller can be use for single output? If yes, Can you share any reference.
Part Number: LM5143 Tool/software: I want LM5143 Pspice average model for simulation.
I design a current loop for charge battery,I need model for simulation.
Schematic as below:
Part Number: LM5143 Other Parts Discussed in Thread: LM5148 , LM5190 Tool/software: hi sir
I Can't find the key word" CC or constant current " in the data sheet of LM5143 & LM5148
if the two parts support the function
need spec as below
…