Part Number: LM5143-Q1 Other Parts Discussed in Thread: LM5143 , LM5170 Tool/software: I am using LM5143 in IBB configuration like the diagram below. Would the controller be able to support current flow in the opposite direction? The customer is curious…
Part Number: LM5143 Tool/software: Hi,
I'm going to use LM5143 to generate single output (10Vin to 3.3V @ 30A). Is this buck controller can be use for single output? If yes, Can you share any reference.
Part Number: LM5143 Tool/software: I want LM5143 Pspice average model for simulation.
I design a current loop for charge battery,I need model for simulation.
Schematic as below:
Part Number: LM5143 Other Parts Discussed in Thread: LM5148 , LM5190 Tool/software: hi sir
I Can't find the key word" CC or constant current " in the data sheet of LM5143 & LM5148
if the two parts support the function
need spec as below
…
Part Number: LM5143-Q1 Other Parts Discussed in Thread: LM5143 , LM5137F-Q1 , LM5137-Q1 Tool/software: Hi,
In datasheet of LM5143, absolute maximum input voltage (Vin to PGND) was given as +70V. Can I know how long (transient condition) the IC withstands…
Part Number: LM5143 Tool/software: Hi,
According to datasheet Fig9-10 for single output with multi-phase application, may I check whether it could support 18V~48V input and 12V/60A output?
Suppose it may be okay, but want to double confirm with team…
Part Number: LM5143 Tool/software: Hello TI experts,
The project we designed used the LM5143+4pcs MOSFET dual phase architecture. input=16-32V ,output voltage= 14.4V, the current max 20A. The output current can reached 12A. Schematic as attached. There…