Part Number: LM5146-Q1 Hello,
On page 31, in Table 9-2 of the datasheet of LM5146-Q1, the power stage zero formula is mentioned as below (in red circle) -
I think the formula is wrong, it should be wL = Rdamp / LF, because this can make inductive…
Parth Shrivastava said: Actually, the Simulation File is a bit confidential, but I can share the Graphical Results with you
Can you atleast share an image of the LM5146 side of things?
If you dont want to post it on the forum - I have sent you…
Hello Kotaro
Kotaro Suzuki said: C15 is placed close to the IC, but is wired with a thin wire on the inner layer.
Device won't carry much current; it will in few mA. Thus, you don't need thicker trace. Following circuit comes in input power…
Part Number: LM5146-Q1-EVM12V Other Parts Discussed in Thread: LM5146 Tool/software: Hi support team
I am using LM5146 evaluation board and measuring CISPR25 conduction current method. However, it is failing above 30MHz. Could you please give me some…
Part Number: LM5146-Q1 Other Parts Discussed in Thread: LM5146 Dear TI, Our requirement is:
BUCK Converter Non Isolated Input Voltage = 150VDC to 275VDC Output Voltage = 140VDC( or adjustable e.g. 100VDC to 150VDC) Output Current = minimum 0.5A or more…
Part Number: LM5146-Q1
I am designing a power architecture for a multi-board system and need guidance on selecting a suitable PWM buck controller and overall power distribution approach.
My system has an unregulated input , which is first converted…
Part Number: LM5146-Q1 Tool/software:
Hello TI Team,
I’m requesting a quick design review for my LM5146-Q1 synchronous buck controller. The application is automotive. Details and files are below. Please let me know if you see any issues or have recommendations…
Part Number: LM5146-Q1-EVM12V Other Parts Discussed in Thread: LM5146-Q1 We were initially planning to use the MOSFETs with part numbers NVMFS6B25NLT1G and NVMFS6B14NLT1G for our iVCU testing, but both of these parts are now indicated as obsolete.
As…
Part Number: LM5146-Q1 Hi
My customer is looking for LTC7899RUFD#PBF replacemnet solution.
Is LM5146-Q1 can do the same as LTC7899RUFD ? or do you have other suggestion ? Thanks
PY Tsai