Part Number: LM5148-Q1 Tool/software: Dear team,
My customer would like to use LM5148-Q1 for their application. please review customer schematic and let me know your opinion.
1. input range : 36V to 60V typ.48V
2. output : 19V/10A , 12V/10A
DCDC_CONVERTER1_R0_240828…
Part Number: LM5148-Q1 Other Parts Discussed in Thread: LM5148 Tool/software: Hello Texas Instruments Team,
I would like to use the LM5148-Q1 for Converting 48V Nominal Input(38VMin-76V Max) to 28V Output.
I would like to know whether we can draw 15A…
Part Number: LM5148-Q1 Tool/software: Will injecting a test signal into the FB pin still work for gain and phase margin testing if the device is configured with a pull-up to VDDA?
If not, how can I test stability?
I'm using a 0Ω pull-up to VDDA to configure…
Part Number: LM5148-Q1 Other Parts Discussed in Thread: LM5148 I am MURAL SELVAM, I need power good signal detection for LM5148-Q1 DC-DC converter, I designed one comparator circuit which does not work properly. my output range is 12V/2A so anyone who…
Part Number: LM5148-Q1 Other Parts Discussed in Thread: LM5175 , LM5176 Tool/software: Hi there,
Currently I am working on development of MPPT based PV optimizer for solar power optimisation,
The Power level of Power optimizer is 700Wp [Voc= 52V, ISC …
Part Number: LM5148-Q1 Other Parts Discussed in Thread: LM5148 , LM5146 , LM5145 Tool/software: Hi Team,
I am planning to use the LM5148-Q1 controller for an automotive buck DC-DC converter and wanted to confirm the meaning of the listed maximum load current…
Part Number: LM5148-Q1 Other Parts Discussed in Thread: TPS25984 , LM5148 Tool/software: Hello,
I am working on a DC/DC buck converter for automotive application using LM5148-Q1 buck controller. Since the application has high safety/reliability requirements…
Part Number: LM5148-Q1 Hi team,
I have been trying to build a Buck converter using the LM5148-Q1 IC. I have made all the calculations and tried to manage any difficulties faced. Still there is just one issue that I have not been able to identify why is…
Part Number: LM5148-Q1 Other Parts Discussed in Thread: LM5148 , LM5149 , LM5143 Hello,
I'm looking for an automotive DC/DC solution with a special load profile: Supply is nom. 48V which need to be converted into 12V. System is always on battery and 12V…
Part Number: LM5148-Q1 Other Parts Discussed in Thread: LM5148 Hi,
A follow up question on previous post.
I have attached the below two pictures just to hear if anybody can confirm if these look OK. They show the switch node (SW) rising and falling edge…