Part Number: LM5152-Q1 Hello, My customer plans to use LM5152-Q1 for their new design and has some questions as follows. Q1: Datasheet Figure 10-4 shows efficiency vs. IOUT, VOUT = 8.5 V, at Vin = 5.5V to 7.5V range. They would like the plots at Vin(min…
Part Number: LM5152-Q1 In our application we use Diode Emulation (DE) Mode for Light Load conditions.
Where is the transition point between "Light Load" and "Not Light Load"?
Part Number: LM5152-Q1 Other Parts Discussed in Thread: LM5152EVM-BST hi Friend,
In the datasheet, I want to know the efficiency on the VIN=18V, Please provide it. thanks
Part Number: LM5152-Q1 Hello Texas Instruments
I am using LM5152-Q1 Pspice Transient Model which changed MOSFET , resister , capacitor and inductor.
I want to check Phase Compensation and Gain margin in my simulation model .
Could you please show…
Part Number: LM5152-Q1 hi Friend,
When the IC output is low voltage, is it achieved by frequency reduction or other ways? In addition, if the output is high voltage, the IC is adjusted by what working principle?
Part Number: LM5152-Q1 Other Parts Discussed in Thread: LM51521-Q1 hi Friend,
I want to know the difference between LM5152-Q1 and LM51521-Q1. in the datasheet ,what means of Bypass Operation?
Part Number: LM5152-Q1 Tool/software: Hi Team,
Could you help review LM5152 schematic for HIWAY Auto IVI project?
VIN=13.5V (12V battery)
Vout=24V@5A
TI_POWER.pdf
Regards,
Sveinn
Part Number: LM5152-Q1 Hello
I would like to ask three questions regarding the specifications of the LM5152-Q1.
Q1.
Please tell me about the configuration mode of LM5152-Q1.
I checked the input voltage, output voltage, high-side and low-side…