Part Number: LM51551 Other Parts Discussed in Thread: LM5155EVM-FLY ,
Hi,
This is a follow-up to the following thread, because I am currently not able to reply to the original thread due to a posting issue.
Original thread:
https://e2e.ti…
Part Number: LM51551 I have designed an isolated flyback converter around the LM51551. Both input and output voltages are 24V with a maximum output of 1A. I found that the IC goes into hiccup recovery mode when it reaches the desired output voltage and…
Part Number: LM51551 Tool/software: Hi Sir,
Our customer is testing their board and they can't get enough current at the output load: There is 56V at output with no load, and the output is drop (protect?) when the current load is more than 500mA.…
Part Number: LM51551 Other Parts Discussed in Thread: LMP8646 Hi expert,
I am designing an application for current limiting with a capacitive load, where the capacitor voltage can be controlled.
The key objectives of this design are:
Programmable…
Part Number: LM51551 Looking for an boost IC to provide the following:
Vin = 16Vdc to 35Vdc
Vout = 48Vdc
Iout = 30A
SWfreq = =/> 500KHz
AEC-100 or AEC-101 certified
Operation Temp. -40C to 125C
nice to have protective features built in the…
Part Number: LM51551 Tool/software: Hi,
We are currently evaluating the LM51551 for our application and have a question regarding the hiccup mode behavior.
According to the datasheet, LM51551 initiates a hiccup mode restart after detecting 64 cycles…
Part Number: LM51551 Other Parts Discussed in Thread: PMP22764 , Hi Team,
Based on the PMP22764 reference design, we would like to use the LM51551 series to design the following spec:
Vin=9v~36V, Vout=54V/ Pout 40W, and need isolate,
if we follow…
Part Number: LM51551 Other Parts Discussed in Thread: PMP22764 ,
Tool/software:
Hi Sir,
We've ever ask LM51551's question earlier and they check PMP22764's design as reference. Customer want to confirm what's the D7 function in PMP22764, and if…
Part Number: LM51551 Other Parts Discussed in Thread: LM5155 Dear Support Team
In the the application note "How to Design an Isolated Flyback Using the LM5155" SNVA866A, a bridging ceramic capacitor between primary and secondary side is used (see C28…
Part Number: LM51551-Q1 Hi team,
Can LM51551-Q1 support 15V@2.5A output @ VIN=9-18V? If not, please recommend a new suitable device.
Target EE is traction inverter.
Regards,
Sky