Part Number: LM51551-Q1 Dears:
Customer want to know LM51551-Q1 leading edge blanking time, I can't find it in datasheet. Could you please hlep provide it ? Thanks.
Part Number: LM51551-Q1 Hi team,
Can LM51551-Q1 support 15V@2.5A output @ VIN=9-18V? If not, please recommend a new suitable device.
Target EE is traction inverter.
Regards,
Sky
Part Number: LMR16006Y-Q1 Other Parts Discussed in Thread: LM51551-Q1 , LM51551 , LMR16006 , TPS560430-Q1 , TPS560430 , LM5155 Hello TI team,
I’m Ali, an external HW engineer at Emotors, I am currently working on a power supply architecture using…
Part Number: LM51551-Q1 Other Parts Discussed in Thread: LM5155 Hi Ti Expert,
About the LM5155(1)/56(1)-Q1 series,
We plan to add some testing point on IC's pinout for ICT.
Is there any specific requirement for this part?
For example, maybe…
Part Number: LM51551-Q1 Hi support team,
We plan to design a 12 V→165 V, 5 W converter for supercapacitor charging. We are evaluating the LM51551-Q1 as the boost controller. However, we are facing the following issues:
The IC’s duty cycle is at…
Part Number: LM51551-Q1 Tool/software:
Hello,expert
please check the Quickstart_Calculator for SEPIC, cell H23, "Peak inductor current, ILPK=ISW_peak_VIN_min", for me, Peak inductor current should be "ILA_avg_VIN_min+ILArip_VINmin".
Part Number: LM51551-Q1 Tool/software: hello
i checked the LM51551-Q1 DATASHHET ,the following PICTURE
As we can see from the following figure, when VCC exceeds 4.5V, the voltage of SS pin starts to rise,but refer to the Red Arrow Position,
When…
Hi Sidharth,
Thanks for reaching out.
Sidharth Gupta said: Is LM5155/LM5156 suitable as a suitable PWM controller IC for for non-isolated, non-synchronous, single MOSFET DC/DC boost converter.
Yes, in general, LM5155 is made for applications like…