Part Number: LM5156 Hi,
We use LM5156DSSR for the boost circuit, when it power on, the configuration of this spec. is not enabled, but it will
output for a few seconds before burning out, please check the schematic diagram that if there are any error…
Part Number: LM5156 Hello, I'm simulating a secondary-side regulated isolated flyback circuit with an LM5156 in PSpice for TI. Unfortunately, different ground symbols in this program are still connected to each other and aren't truly isolated. How can…
Part Number: LM5156 Hi Ti, I want the clock of the LM5156 to be generated by a microcontroller. So it would be possible to adjust the clock on the fly. Is that possible and how to interface with the SYNC input. kind regards.
Part Number: LM5156 Other Parts Discussed in Thread: LM5155 , Hi,
I would like to ask you to review whether my use of the LM5155/56 Flyback Design Tool is appropriate for the following customer requirement.
The customer requirement is:
- Topology…
Part Number: LM5156 Hi,
Please help to check our LM5156 design and Quickstart_Calculator tool, and advise if there are any error for this design, thanks.
lm5156DSSR.pdf
LM5156_Excel_Quickstart_Calculator_for_Flyback_Regulator_Design.xlsx
Part Number: LM5156
Hi,
I would like to confirm whether my understanding is correct.
The customer requirement is as follows:
- VIN = 42 V
- VOUT = 5 V or 24 V
- IOUT = 2 A minimum, preferably 3 A or higher
- Maximum power case: 24 V /…
Part Number: LM5156 Dears,
I have a design requirement to let "www.ti.com/.../snvu736.pdf" to support wider input range.
My target is to have a 9~54V input flyback design for 5V/3A output usage. Could you share the design modification for me?
…
Part Number: LM5156-Q1 Other Parts Discussed in Thread: LM5156 Flyack converter designed for Vin input voltage from 6V to 16V and power output of 14W. At start when the flyback converter was having minimum load, it was going unstable and after observing…
Part Number: LM5156 Hi,
One of our customers is currently evaluating LM5156 / LM51561 for an isolated flyback DC/DC power supply. The customer is considering the following two design conditions:
Case 1:
Device: LM5156DSSR or LM51561
Topology:…
Part Number: LM5156 Other Parts Discussed in Thread: LM5155 HI team,
Customer is considering to use LM5156 for SEPIC converter to generate 24V/2A from 12V~48V.
They downloaded LM5155_56_Excel_Quickstart_Calculator_for_SEPIC.xlsx, but the input box…