Part Number: LM5156 Other Parts Discussed in Thread: SN74LVC3G14 , LMG2100R044 , Hi
The circuit diagram is designed with the following specifications.
-SPEC-
Input: dc24V
Output: dc 80V 5A
Part: LM5156,LMG2100R044,SN74LVC3G14
I'd like to get a review, but…
Part Number: LM5156-Q1 Other Parts Discussed in Thread: LM5156 Hi Team,
I am simulating the LM5156-Q1 using Lt-spice but I am not getting the gate voltage in simulation.
Please can you check and let me know? What issue is the issue I am facing let me…
Part Number: LM5156 Hello Experts, I create the desing to generate 90V using LM5156. I use the same design from the WEBENCH
I took this design and simulated in the LTSpice.
For some reason the Vout is 22V for LTSpice, whereas in the WEBENCH is 89V.
…
Part Number: LM5156 hi sir
i would like to design a dc-dc power stage, spec as below, LM5156 is a right solution?
For Positive, +10V~+110V Vout programmable, 48Vin, Continuous 0~40V /2A, Transient 110V/2A
For Negative, -10V~-70V Vout programmable, 48Vin…
Part Number: LM5156 Hello Team,
We use LM5156 to design a boost circuit, Input: 8.8V, Output: 12V/4A.
But now the inductor and MOSFET is too hot. What should we do to improve this circuit?
Thanks!
Part Number: LM5156 Hi I am building a flyback converter based on the LM5156. It is supplied by 15v and I have it set to switch at 100 khz (94% duty cycle). When probing the gate I can see a 100khz square wave but the gate is not actuating when I am using…
Part Number: LM5156 Other Parts Discussed in Thread: LM5155 , , LM555 Hi,
I'm trying to design a boost converter to have 300VDC in the output from 12VDC (regulated) in the input, so I was thinking on using the switching controller LM5155/LM5156. For this…
Part Number: LM5156 Other Parts Discussed in Thread: LM5155EVM-BST ,
for EVM: LM5156EVM-BST, or LM5155EVM-BST PCB, :
What is the total thickness ?
What is the thickness for each layer ?