Part Number: LM5156H Tool/software: Hi,
I designed flyback converter, based on the LM5156H.
Input Voltage = 12V
Output = 56V/600mA
Transformer:
Np/Ns/NAUX = 9T/30T/5T
Lp = 12uH
L,Leakage = 0.1uH
Freq.Sw = 250KHz
It will be great if you…
Part Number: LM5156H-Q1 Other Parts Discussed in Thread: INA199 , LM5156 , PMP10081 Tool/software: Hi, I am working on a concept to make a constant current flyback converter.
My idea:
Use INA199 to sense the current from an Rsense connected in series…
Part Number: LM5156H Other Parts Discussed in Thread: PMP22764
Tool/software:
Hi,
I've designed an isolated flyback circuit, which gets 12V and outputs 56V/600mA.
I used PMP22764 as a reference design, and modified it.
Schematics:
Flyback_Sch_040325…
Part Number: LM5156H Other Parts Discussed in Thread: LM51561H , LM5156 , TPS61087 Tool/software: Hi all,
I'm developing a boost converter for LEDs, based on a Webench simulation of the LM51561H. I incorporated modifications aligned with Figure 10-9…
Part Number: PMP20212 Other Parts Discussed in Thread: LM5156H , LM3481 , , LM5156 Tool/software: Hi team,
I would like to make the exact same reference design as the PMP20212, however using the LM5156H instead of LM3481.
Will this be possible?…
Part Number: LM5156H Other Parts Discussed in Thread: LM5156 Dear TI team, I've designed a boost converter using the LM5156 IC with an input voltage of 50V, output voltage of 180V, and an output power of 30W. The converter's frequency is set at 330kHz…
Part Number: LM5156H Hi,
I would like to build a flyback converter around the LM5156H controller. The links of the guide and calculator on the datasheet are not working. Can you send me a copy of these guides:
Thanks.
Part Number: LM5156H-Q1 Other Parts Discussed in Thread: LM5156-Q1 Tool/software: Hi team,
My customer is using LM5156-Q1. They want to know whether a short-term (100us) power failure (Vsupply drop) will affect secondary output. Could you share some…
Part Number: LM5156H Tool/software: Hello,
I used webench to design voltage booster that provides 270Vdc 700mA with LM5156HPWPR. Also I need to trimmer the output voltage as suggested in device datasheet (Figure 10-7). The output should be changed from…
Part Number: LM5156H-Q1 Tool/software: Hello Team,
I am working on LM5156HQPWPRQ1 PWM controller IC. And I have seen that IC is malfunctioning.
when voltage is given externally at EN (pin 14), seeing voltage at BIAS (pin 1) pin. So, I want to understand…