Part Number: LM5156H-Q1 Other Parts Discussed in Thread: LM5156-Q1 Hi team,
My customer tried to simulate LM5156-Q1 on PSPICE for TI.
Customer uses below model which is downloaded from the product folder.
"Unencrypted LM5156-Q1 PSpice Transient Model Package…
Part Number: LM5156H-Q1 Other Parts Discussed in Thread: LM5156 , LM51561H Hi
Please answer the customer's questions. 1) What happens when OUT PUT 12V Line Short occurs?
(Recovery enabled?, Converter damaged? Maximum sustainable time?)
Part Number: LM51561H-Q1 Other Parts Discussed in Thread: LM5156H-Q1 , LM5156 Hello Flyback Controller Team,
My customer try to use LM5156H-Q1 with PSR fly-back.
The load current (secondary side) is very wide as 50mA to 600mA, does LM5156 have pulse-skip…
Part Number: LM5156HEVM-FLY Other Parts Discussed in Thread: LM5156H-Q1 Hi
While I test LM5156HEVM-FLY, I have a question about that.
1.I checked and tested EVM, but it has a difference from what I think. Originally, Vsw is Vin + Vor(Reflected output…
Part Number: LM5156
Dear *,
can you tell what is the difference between those devices ?
LM5156, LM51561
LM5156-Q1, LM51561-Q1
LM5156H, LM51561H
LM5156H-Q1, LM51561H-Q1
Also which of these devices have spice model for BOOST simulation?
And what is the…
Part Number: LM5157-Q1 Other Parts Discussed in Thread: LM5157 , LM5156H , LM5156 Hello support team,
Customer would like to do WEBENCH simulation for LM5157 SEPIC design, however, WENECH does not support it. Do you have any plan to support?
I found WEBENCH…
Part Number: LM5156H Other Parts Discussed in Thread: TIDA-050023 , LM51551-Q1 Hello,
I try to design a PoE++ converter with 12v@4.5A (54W) output. I want to use TPS2372-4 and LM5156H for that (similar to reference design TIDA-050023 ).
I followed the design…
Part Number: LM51561H-Q1 Other Parts Discussed in Thread: LM51561H , LM5156H Hi
Please review the customer's schematic
1. In the case of EVM, Out Put GND is to be Isolated. Is there any problem with the schematic layout?
2. In case of D1, it is designated…
Other Parts Discussed in Thread: LM5156H , LM5155 , LM5156-Q1 Dear *,
please can you suggest a device for 50V-200V Boost converter for pulsed discharge application (Adj Out Voltage)
Vin 24V
Vout from 50V to 200V
Iout from 0.3A( for 50V) to 0.075A ( for 200V…