Part Number: LM5158 Tool/software:
Dear Engineers,
I have designed a variable-output boost DC-DC converter (LM5158RTER) to step up 5 V to 40 V. However, after receiving the PCB, I noticed that the output is fixed at 4.98 V, even when adjusting…
Part Number: LM5158 Other Parts Discussed in Thread: LM5185 Tool/software: Hi Team,
May I check if LM5158 can support PSR voltage feedback like LM5185? customer want reduce one aux channel.
Thanks & Regards
Eddie
Part Number: LM5158 Other Parts Discussed in Thread: LM5157 Dear TI,
I used the Webench software to create a design for an isolated flyback converter. The IC used is LM5158RTER. The design converts unregulated nominal 24V input voltage (min..max 16V…
Part Number: TPS2663 Other Parts Discussed in Thread: LM5158-Q1 , , LM5158 Hello,
Our board is supplied by two 28V power supplies.
These 28V power supplies each goes through a TPS26631 and are then interconnected thanks to diodes as a 28V internal…
Part Number: LM5158 Other Parts Discussed in Thread: LM5121 Hi,
for my application I'm looking for a boost controller with inrush limiting. At the output of the controller we have to use and buffer capacitor with 300uF for power cut purposes, but on…
Part Number: LM5158 Do you have a SEPIC converter which can operate at 1 to 1.5Vdc input voltage and provide 6 to 7 Vdc output voltage?
Meanwhile, it has the spread spectrum feature to provide the optimal EMI performance.
Part Number: LM5158 Tool/software: on behalf of my customer:
The LM5158 is used as a 48V PoE supply for the master (24V --> 48V). With PoE, there is a voltage limitation at 57V. In many PoE Slave designs I see a 58V Zener diode to limit the maximum…
Part Number: LM5158 Tool/software: Hi, Staff
I'm designing boost convertor.
Vsupply range is from 25.5V to 46.0V
Vload range is from 47.05V to 49.96V.(Typ. 48.5V)
Target Fsw is about 500KHz.
In Vsupply is 46.0V and Vload 47.05V, PWM Duty is…