Part Number: LM5158 Tool/software: I want to design an isolated power circuit with a 10–60V input and 12V output. When I use Webench the attached design seems suitable, but here the input GND and the output GND are the same. I think this would break the…
Part Number: LM5158
Tool/software:
Hello,
We are intending to use the LM5158 to generate a 45V regulated power supply from our 20V to 32V input power supply.
The 45V is used to generate further secondary supplies and to cope with the potential…
Part Number: LM5158
Tool/software:
Hi team,
my customer used LM5158 and find that there is an inrush current within a few ms after EN is turned on (but the actual TSS setting is several hundred ms), and the Vout suddenly has a voltage of more than…
Part Number: LM5158 Tool/software: Hello,
I downloaded the boost computation file.
It does not open in Microsoft excel, stating that it is due to the protection. Any hint ?
I was able to open it in Sheets which overrides any protection but I think…
Part Number: LM5158 Other Parts Discussed in Thread: LM5157
Tool/software:
Hello
I have the same issue, the compensation values that are output by Webbench and the calculated suggestion in the sheet differs.
What am I missing ?
webench.ti.com…
Part Number: LM5158 Tool/software: Hello,
I'm working on a 48V to 3x isolated 28V @ 0.2A flyback converter, using LM5158 and a Pulse VPH5-0155-R or Wurth 749196518 1:1:1:1:1:1 transformer with ~23µH primary inductance.
Please could you advise on the…
Part Number: LM5158-Q1 Other Parts Discussed in Thread: LM5157 , LM5158 Tool/software: Dear,
I have filled the LM5158-Q1 boost converter design tool spreadsheet (attached) for a boost with Vinput between 3.4 and 5.25V and Vout=44V. Could you please…
Part Number: LM5164-Q1 Other Parts Discussed in Thread: LM5158-Q1 , , LM5158 , LM5164 , LM65645-Q1
Tool/software:
Hello,
We are having an issue with the LM5164-Q1 and the LM5158-Q1.
We are using a LM5158-Q1 to generate a 45V from our 28V power…
Part Number: LM5158 Hello guys,
One of my customers is looking for a boost regulator which can be used as a power supply for PSE side of PoE.
Their requirements are the follows. Vin=12V or 24V. Vout=37V~57V. Io=0.350A. Pout=13W.
I think LM5158 can…