Part Number: LM5158-Q1 Hello,
During testing the test my costumer noticed the following behaviour:
"I noticed some unusual behavior. In certain scenarios, the regulator enters a burst mode. This effect occurs in some operating states but not…
Hi,
thank you for using the E2E forum.
You can have a look at the LM5158 (converter) of the LM5156 (Controller).
For both there is also a Flyback EVM available
LM5158EVM-FLY Evaluation board | TI.com
LM5155EVM-FLY Evaluation board | TI.com …
Hello Steve,
Thanks for reaching out. Yes, you are right, the LM51581 can be used as a Flyback too and the only difference is that it has a lower peak current limit than the LM5158. I would suggest to use the Excel QuickStart calculator as a starting…
Hi Stefan,
Actually, The simulated parameter is set according to the LM5157 flyback-EVM that I requested in ti.com. The compensation loop is designed by the application note which can also be download in ti.com (see attachment). The C_COMP is 22nF,…