Part Number: LM5160 Hi Team
The frequency of the output voltage from LM5160 does not match the set frequency (400 kHz). Please help check the circuit.
Figure1: SCH
Figure2: Output voltage frequency (Input=9.6V)
Figure3: Output voltage frequency…
Part Number: LM5160 I have an LM5160 in a Flybuck supply. The primary side is not isolated from a motor drive inverter with heavy switching noise. As a result, I have seen the LM5160 generate spurious switching pulses that coincide with the inverter switching…
Part Number: LM5160 Tool/software: I am working on the design with LM5160/LM5160A. Is it possible to get the design files of the LM5160DNTFBKEVM board?
Part Number: LM5160 We are testing a brownout scenario where the input voltage to the flybuck dips below the UVLO of the LM5160. Because the input voltage is not well-regulated, it quickly ramps back up above the turn-on threshold after the LM5160 shuts…
Part Number: LM5160 Other Parts Discussed in Thread: TINA-TI , Hi,
I would like to make a circuit with VIN=12 V and VOUT=-12 V using TINA TI. I have the circuit I made, but it cannot output the desired voltage. Could you tell me where to correct it…
Part Number: LM5160 Tool/software: Hi Team,
Can the LM5160 meet the below condition? Input voltage: 9~36V, output voltage: 12V, Current: 1A, Industrial specification (-40~85)
Part Number: LM5160 Tool/software: In mode3 in the figure,:t3: the primary current is negative, which can be understood, but why the current is positive at time t0, I don't understand this switching path。
www.ti.com/.../ssztcb7.pdf
Part Number: LM5160 Other Parts Discussed in Thread: LM5161 (1) LM5161: The power output affects the accuracy of sensor - Simulation, hardware & system design tools forum - Simulation, hardware & system design tools - TI E2E support forums
Our application…
Part Number: LM5160-Q1 Tool/software: Hello,
We have flybuck topology as attached in the schematic. Output voltage ~15V and load at the secondary output approx, 200mA. (2.5W~3W max). 15V used for Gate switching of Inverter IGBT (16kHz switching…
Part Number: LM5160-Q1 Tool/software: Dear TI Support Team,
We are using LM5160QPWPRQ1 part. Refer SCH here:
https://community.nxp.com/t5/S32K-Knowledge-Base/Automotive-Electrical-E-compressor-Aircon-RDB-based-on-S32K142/ta-p/1414316
But turn-on…