Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM5160 , LM25184 Hi!
I am looking for more, possibly higher current alternatives (~2.5 to 3A) to LM5160-Q1 IC in fly-buck configuration.
Can anyone suggest other buck ICs that can be comfortably used…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM25183-Q1 , , LM25183 Hi Sir,
My customer is looking for a isolation power devices to meet the ISO 7637 standards, and the power spec V-in is 9~36V, V-out is 12V, I-out is 2A. They found these devices…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM5160 Hi,
The customer applied LM5160-Q1 to the new project.
Please review the schematic and give us advice.
Topology option : Flybuck
Input voltage: 10.5V~16V
Output voltage : 15V
Output Current…
Part Number: LM5160-Q1 Hi team ,
Our design used the " LM5160-Q1 " IC , Fly-Buck topology ( used planar Transformer ) ,
I need to calculate the rise time / fall time of the converter output ( single output ) , please help me to calculate the…
Part Number: LM5160-Q1 Hello tech support,
We have purchased this device from TI store,but there exhibit contamination and scratches on the device body
What is the problem with that?
Does it meets all the datsheet specs such as fit and reliablity?
Could…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM5160 , PMP Hi Teams,
Recently, I studied the reference design named PMP32077 whose topology is Fly-Buck-Boost.
There is a question on absolute ratings of FB to AGND in powering LM5160-Q1 initially…
Part Number: LM5160 Hello,
Can someone help me fill in/check this table please:
MPN
MFR
Function/Topology
Max. Output Current
Output-Input Type
Output Polarity
Output Voltage
LM5160DNTT
TI
xx
xx
Adjustable
Positive
2-50V
Please select from…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM76005 , LM76003 , TPS54561 , TPS54560B Hi team,
Could you give me comment on following customer question?
Q1. Does TI have alternative option for higher output current of LM5160Q1?
The output current…