Part Number: LM5160-Q1 Hi experts,
My customer would like to transfer the voltage from 52V to 12V/1A or 24V/0.5A, both 12V /1A and 24V /0.5A are fine.
I would like to know is there any pros and cons between 12V and 24V? like inductor space or efficiency…
Part Number: LM5160-Q1 Hi
My customer evaluate LM5160-Q1 as Fly-Buck converter.
They are trying to reduce the radiated noise on thier board.
They put the resister in series with boot capacitor.
Are there the recommending value of that resister…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM5160 , TCAN1043 , TCAN1043-Q1
Hi Team,
The customer has drawn up a schematic for EN control.
I connected TCAN1043 INH pin and LM5160 EN pin directly, is there any problem?
TCAN1043-Q1 INH…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM5161-Q1 Dear support member,
My customer used LM5161-Q1.
I have a question.
(Situation) My customer want to measure the phase margin and gain margin to verify the feedback stability of the…
Part Number: LM5160-Q1 Hi Team,
could you explain why it says "The primary-side output voltage of a Fly-Buck converter must be no more than one half of the minimum input voltage."?
thanks a lot.
Yang
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM5160 Hello,
I want to build a flybuck converter with LM5160-Q1. I have done some simulation work and the result shows that the output voltage could be controlled.
But I notice a minor problem…
Part Number: LM5160-Q1 Hello, I have use LM5160-Q1 to make an isolated flybuck converter. The circuit is shown below.
The simulation result looks good. It can control the output voltage to its target value and the process looks nice.
As you can…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LMR33630 Hi Team
I want to calculate the smallest Vin when Vout is fixed by the formula here.
Vout=Vin*(tsw-toff_min)/tsw
Since the datasheet only shows the Typ value of toff_min, I would like…
Part Number: SN6505B-Q1 Other Parts Discussed in Thread: LM5160-Q1 , LM5160
Hi Team,
What’s the difference of output-regulation-performance between Flybuck and Push-pull ?
The use-case is CANbus module as below shows:
A simple comparison table…