Part Number: LM5160A Hi
I'm designing a Flybuck DC-DC converter using the LM5160A. The design has an input voltage in the range of 25 V to 45 V. I have designed for an output of 12.5 V on the primary side and 14 V on the secondary side. I simulated…
Part Number: LM5160A My customer has the following questions:
I’m intrigued by the “Flybuck” topology. I have a couple questions regarding it.
It appears the GND/references are isolated between the primary and secondary sides. Is it required for…
Hello Mattia,
For the Transformer stack, I suggest the following.
The Primary should "sandwich" the secondary's. By this, I mean, winding half the primary first, then insert the secondary's and then finish off the second half of the primary. I would…
Part Number: LM5160A
Customer just downloaded and tried to use this design tool (Calculator_Rev1p03.xlsx) from the website. However, the user cells for compensation components (cells B120, B122, B124, B126, and B128 on tab Fly-Buck-Boost) are permanently…
Betty,
Flybucks have limitations on maximum duty cycle based on the leakage inductance of the transformer. See this document, especially figure 4 . This may be your issue more than the output capacitance.
-Sam
Part Number: LM5160A Other Parts Discussed in Thread: LM5160 Hi,
I'm trying to generate a negative 12V output from a +12V input using the LM5160A, but am finding it cannot supply the 500mA I need without going unstable. Please can you have a check…
Part Number: LM5160A Other Parts Discussed in Thread: LM5160 , TIDA-00199 Hi everyone,
I have question about GT03-122-037-B transformer model of Ice Components, This transformer have 2 seconder as 1:2.5:2.5. I am planning to obtain 20V and -5V for driving…
Part Number: LM5160A Other Parts Discussed in Thread: PMP , LM5160 Hi, team.
I often reference the following devices and documentation when introducing isolated DC/DC.
Devices: LM5160A
TI-design document: www.tij.co.jp /.../ PMP 10532
So question…
Part Number: LM5160A Other Parts Discussed in Thread: TINA-TI , LM5160
Tool/software: TINA-TI or Spice Models
Hello everyone,
I am using the LM5160 to create 20V and -5V isolated supply.
Vin=24V,
Soft start=30ms,
after 30ms I have resistors…