Hello,
When I open the datasheet, I see the output current is rated to 2A.
For example flybuck designs, there are multiple reference designs on the Tools Tab, including: www.ti.com/.../PMP15005. You can also see the EVM with the flybuck configuaration…
Part Number: LM5160A Other Parts Discussed in Thread: LM5160 , LM5160DNTFBKEVM , PMP10532 , PMP Hello,
I'm using an LM5160 for a two output isolated flybuck. It is converting from 10-40 Vin to 3.3 Vout for all outputs (the isolated and non isolated one).…
Hi Aravind,
there is an existing evaluation board for LM5160 for isolated Fly-Buck application www.ti.com/.../lm5160dntfbkevm and user guide www.ti.com/.../snvu408a.pdf you can share with your customer to look at.
Best Regards,
Robert L
Part Number: LM5160 Other Parts Discussed in Thread: LM5161 , LM5017 , Hello,
My customer needs an isolated 12V @ 30mA design with input range 9 to 18VDC . I sent the LM5160DNTFBKEVM with the recommendation to change R6 to 56k. The customer has done this…
Part Number: LM5160 Hi,
I'm evaluating LM5160 on LM5160DNTFBKEVM (Flybuck topology) and set external components based on calculator as attached.
LM5160FBKQuickStartCalculator - FinalVersion 20190625.xls
VIN=24V, Vout-pri=12V, ; Iout-pri=0A, Vout-sec…
Hi Steve,
At V CC < 5.5V (V IN <~5.6V) the high-side peak current detection becomes noisy.
In this case the current limit detection is sensed on the low-side FET.
When the lowside MOSFET measures over-current it will extend the off-time until the…