Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM5161 I am designing a variable output voltage converter. The input voltage range is 20 - 50VDC. The output is variable from 0V to 12V @ 0.5A. Is the LM5161 a viable candidate for this design or…
Part Number: LM5161-Q1 Hello experts,
according to TI website the LM5161-Q1 provides the feature "No External Ripple circuit needed (at FPWM = 0)". Also the datasheet says "When the FPWM pin is grounded or left floating, an internal ripple injection circuit…
Part Number: LM5161-Q1 Hi Team,
Customer want to use LM5161-Q1 as Flyback, but the Webench tool only has Flybuck choice.
So customer wonder if we have Excel tool/ App note or other document to help them calculate the components?
Thank you!
Marc
Part Number: LM5161 Other Parts Discussed in Thread: LM5160-Q1 , LM5160 Hi Team,
Can LM5161 replace LM5160-Q1 directly? 1A switching current is enough for customer, and it`s industry application, so no need for Q1 version.
And could you help share the…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM5161 Hello,
I am working with the LM5161 chip in the flybuck topology. We area using type 3 ripple injection for controlling on and off time for the constant on time control. The issue we are having…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM5161
Hello, I Am using a flybuck topology design for the main supply in my main design. While using webench power designer, I wish to change the transformer being used. While looking for alternatives…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: UCC28C45-Q1 , UCC28C45 Dear Sir,
My customer consider as below spec using LM5161-Q1.
Could you please check it possible or not.
1. if possible, could you provide reference schematic and let me know…
Part Number: LM5161-Q1 Hello,
When a reverse current hits the low-side sinking current limit I SINK(LS) , while the V OUT is kept higher in CCM, for example, how will an LM5161-Q1 behave? Will it move to an ON-time state?
Best regards, Shinichi Yokota
Part Number: LM5161-Q1 Hi, Team,
I want to design the Buck with this part.
Question
-How much MIN and MAX of Toff-min spec does the device have under following conditions?
Fsw: 400kHz
Vout: 15V
Iout: 550mAmax
Vin(min): XX V(we want to make sure how…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM5161 Hello,
Can a Fly-Buck converter with LM5161-Q1 start up successfully with a VIN of fast ramp of about 100 V per 20 to 30 µs? Some tests suggest the LM5161-Q1 draws a high rush current with…