Part Number: LM5161-Q1 Hi,
We got a question from customer about LM5161-Q1. Could you help us?
[Question] How much is the recommended minimum switching frequency under the following condition?
Topology: Fly-Buck-Boost Vin=5~20V Vpri=-8V Ipri=0A Vsec1=15V Isec1…
Part Number: LM5161-Q1 Hello,
Please i need your support
I have 2 questions.
1. Question:
8.2.1.2.5 Output Capacitor Selection: they have ripple voltage ΔVO = 10 mV, how do you get there?
for my application which value should I take ?
2. Question…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM5160DNTFBK-CALC Hi TI,
I have an application which will use LM5161-Q1 in a fly-buck configuration. I'm testing a few custom transformers and have the design working but I'm not sure if the temperature…
Part Number: LM5161-Q1 Hi,
We got a question from the customer about LM5161-Q1. Could you help us?
[Question] How is determined ON time in current limit mode? They want to culcurate the output current in current limit mode.
They assume the ON time is determined…
Part Number: LM5161-Q1 Hi Team
can we use Vout = 5V at Max Vin = 58V ?
such case duty is too small at Max Vin =58V,
so that I would like to ask BU's opinion.
Part Number: LM5161-Q1 Hi,
We got a question from the customer about LM5161-Q1. Could you help us?
[Question] They found the distortion at the rising edge of SW node waveform. Please refer to attached file for the detail. We would appreciate it if you could…
Part Number: LM5161-Q1
Hi,
We got a question from the customer about LM5161-Q1. Could you help us?
[Question] They found the primary side transformer current hit the current limit of the IC at the start-up. Please refer to attached file for the details…
Part Number: LM5161-Q1 Hello.
I have a question about the LM5161-Q1.
When shut down, how much is the current flowing through the RON pin? Do you control current flowing in? Data sheet P9 Referring to Figure 15, the impedance of RONPIN is low impedance of…
Part Number: LM5161-Q1 Hi,
We got a question from the customer about LM5161-Q1. Could you help us?
[Question] - How much is the variation of TRES and current limit forced Toff under the following condition?
Vin=24V and 48V Ron=100k Ta=-40, 25, and 125C Vfb…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM5161 Hi
My customer look for Fly Back converter the following condition.
I will propose LM5161-Q1 with Fly-Buck topology.
Could I use this device under that condition?
Vin=8~16V
Vout=15V
Iout_max…