Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM5161 Hi
My customer look for Fly Back converter the following condition.
I will propose LM5161-Q1 with Fly-Buck topology.
Could I use this device under that condition?
Vin=8~16V
Vout=15V
Iout_max…
Part Number: LM5161-Q1 Hi,
We got a question from the customer about LM5161-Q1. Could you help us?
[Question] - How much is the variation of TRES and current limit forced Toff under the following condition?
Vin=24V and 48V Ron=100k Ta=-40, 25, and 125C Vfb…
Part Number: LM5161-Q1 Hi,
We got a question from the customer about LM5161-Q1. Could you help us?
[Question] How much is the variation of the constant 1.008*10^(-10) under the following condition?
Topology: Inverting Buck-Boost Vin: 6~32V, 6~20V Vout: 8…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM53635-Q1 , LM5018 , LM25141-Q1 , LM53603-Q1 Hi,
We got a question from the customer about LM5161-Q1. Could you help us?
[Question] According to the datasheet, the operating lifetime is de-rated for…
Part Number: LM5161-Q1 Hi Team
FB pin can have high switching frequency noise easily.
may I ask the internal block for FB has LPF inside to filter out high frequency of switching noise ?
or FB pin is directly connected the input of error amp without…
Part Number: LM5161-Q1
Hi,
We got a question from the customer about LM5161-Q1. Could you help us?
[Question] They evaluated LM5161-Q1 in Fly-buck-boost topology on their own board. Before the IC starts switching in start-up, the negative voltage occurs…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM5161 Hello,
Can you confirm what the maximum frequency capability of LM5161 is?
Page 1 says that it is adjustable up to 1MHz.
My design Vin = 48V and Vout = 12V. According to equations 3 and 4,…
Part Number: LM5161-Q1 Hi
I get the questions from my customer about LM5161-Q1.
My customer use LM5161-Q1 as Fly-Buck converter.
My customer try to calculate entire the supply currents of this device for calculating the Tj.
This device's datasheet…
Part Number: LM5161-Q1 Other Parts Discussed in Thread: LM5161 Hi Experts:
My customer is testing their board with the EMI specification , in the RE test, they found the harmonic frequency 55Mhz, 66Mhz, 77Mhz,88Mhz, which is derived from the 11Mhz…
Part Number: LM5161-Q1 Hi
I have a questions about LM5161-Q1.
My customer use this device as Fly-Buck controller.
But the large serge noise occurs
Generally, I think Fly-Buck topology don't have to add the snubber circuit,
if they add the snubber…