Part Number: LM5163H-Q1 Other Parts Discussed in Thread: LM5163 Hi,
I’m currently using an LM5163 in my design and I have a question about VEN/UVLO-rising and VEN/UVLO-falling. In the datasheet VEN/UVLO-rising is specified to max 1.1V and VEN/UVLO-falling…
Part Number: BQ76952 Other Parts Discussed in Thread: LM5013 , LM5163 , , LSF0204
Tool/software:
Hi team members,
While going through the technical documentation of the Integrated circuit, I found the Failure mode analysis is provided for the buck…
Part Number: TIDA-010216 Other Parts Discussed in Thread: LM5163
UNder which circumstance does FC pin activated, why do we have to change the switching frequency of lm5163.
KIndly help.
Hi,
You will want to look for devices with -Q suffix in their name for automotive qualification.
LM5163-Q1 seems to meet your criteria. Please have a look and let me know if that works.
Regards,
Niranjan
Part Number: LM5168 Other Parts Discussed in Thread: LM5163 , Hi all,
We are designing a battery powered board which will have non-isolated communication as default, and isolated communcation optinal. Since we have limited area on the board, It is important…
Hi Kevin,
What is the output current and desired switching frequency? Please fill the quick-start calculator and get back to us.
LM5163-LM5164DESIGN-CALC Calculation tool | TI.com
Regards
Arpita
Hi Zhanjia
It should be "lesser than or equals to" as per Equation 9 for COT devices.
You may want to go through Selecting an Ideal Ripple Generation Network for Your COT Buck Converter (Rev. A) {Eq 9} for more details. here is the excerpt from the…
Hui Kevin,
here are few comments on the LM5164 part of the schematic
For a typical vin (47V) and given circuit parameters, it is required to use RA=150k ~220kohm range for sufficient ripple at FB node
Please directly connect the EP and GND…
Part Number: LM5146-Q1 Other Parts Discussed in Thread: LM5146 , LM5166 , LMR38020 , LM5164 , LM5163
Hi Team
I need an IC with 0 to 65V input and delivers 3.3V, 5V, 12V outputs. Now I am using LM5166 and LM5146 ICs. Can you suggest me an advancer…