Part Number: LM5163 Tool/software: WEBENCH® Design Tools Hi TI-team
I calculated the following condition using WEBENCH.
Vinmin=30V, Vinmax=90, Vout=15V Iout=0.5A.
In additon, I optimized with Small Footprint Design.
Then Cout is 3.3μF.
The…
Part Number: LM5163 I'd like to use this buck converter on my wireless power receiver PCB to charge batteries. Looking at 130mA max draw from the switcher. My receiver coil (DCR = 2 ohms) generates about 25Vpp max with my resonant cap at about 113kHz…
Part Number: LM5163-Q1 Hi Champs,
there is an abs max rating of the Cbst cap stated in the datasheet. A customer raised some concerns that, with the given tolerances of the standard caps they might exceed the 2.5nF abs max. specification.
Can you…
Part Number: LM5163-Q1 Other Parts Discussed in Thread: LM5163
Team,
do we have TINA model for LM5163-Q1?
The SPICE one which is available shows strange behavior in simulation (in LTspice). It looks like the device was in BOOST current mode without…
Part Number: LM5163-Q1 Other Parts Discussed in Thread: LM5163 Hello,
I’m Gabriel An, working in TI Korea automotive.
This is LM5163 block diagram which is the COT topology.
I knew that Ton starts for constant on-time, when feedback voltage starts…
Part Number: LM5168 Other Parts Discussed in Thread: LM5163 Tool/software: Hi team,
My customer use LM5168 with VIN 30V, VOUT 13.3V, when they increase current load from 0A to 10mA(electronic load CC mode), the VOUT will collapse to very low voltage…
Part Number: LM5163H-Q1 Other Parts Discussed in Thread: LM5163 Tool/software: Hello guys
I am using lm5163H-Q1 to build buck converter, now my customer let us to perform worst case analysis, does there is any tools to do it in fast way?
thanks
Part Number: LM5163H-Q1 Other Parts Discussed in Thread: LM5085 , LM5163 Tool/software: Assuming proper PCB layout is achieved, are EMI filters needed for Constant On Time converters like the LM5163 and LM5085?
If so, can you refer me to any app notes…
Part Number: LM5163H-Q1 Other Parts Discussed in Thread: LM5169 , LM5168 , LM5163 Tool/software: I am trying to determine which converter is best for low current operation. I am looking at the LM5163 vs the LM5168 and LM5169.
It appears the LM5168P…
Part Number: LM5164-Q1 Other Parts Discussed in Thread: LM5164 , LM5163 Tool/software: Hello dear TI team,
In the context of using a buck converter such as the LM5163 or LM5164, is it advisable to incorporate an additional Schottky diode at the switching…