Part Number: LM5163-Q1 Other Parts Discussed in Thread: LM5163 I am considering using the LM5163‑Q1 in my project. My required output voltage is 18 V, with a normal input range of 22–36 V. In the worst-case condition, the input voltage can drop to 18…
Part Number: LM5163-Q1 Hello,
I am using the LM5163-Q1 buck converter in my Motor Control Unit to generate 12V from the Battery voltage of 48V. The generated 12V will be supplied to my Gate Driver Unit which drives the B6 bridge.
What I need are…
Other Parts Discussed in Thread: LM5163-Q1 Tool/software: Dear Sir or Madam,
In one of our products, we are using the following components manufactured by your company:
LM5163-Q1
For a new project our customer has requested us to register…
Part Number: LM5163-Q1 Tool/software: Hi,
In one of our ongoing projects, we are currently using the LM5163QDDARQ1 adjustable buck converter.
We are now considering a change from the adjustable version to a fixed output regulator . We are looking…
Part Number: LM5163-Q1 Dear,
I configured the ic in order to have 12V as regulated voltage output, but the measured output voltage is higer than expected value.
I did the measurement on several boards and the measured values are in the range 12.6V…
Part Number: LM5163-Q1 Dear Team,
The customer has concern about possibility of floating on PCB mount on LM5163QDDARQ1 .
Does it have any floating risk on PCB mount due to stencil thickness of solder paste on lower thermal pad?
Especially, In case…
Part Number: LM5163-Q1 Dear Team,
The customer has concern about possibility of floating on PCB mount on LM5163QDDARQ1 .
Does it have any floating risk on PCB mount due to stencil thickness of solder paste on lower thermal pad?
Especially, In case…
Part Number: LM5163-Q1 Dear Team,
The customer has concern about possibility of floating on PCB mount on LM5163QDDARQ1 .
Does it have any floating risk on PCB mount due to stencil thickness of solder paste on lower thermal pad?
Especially, In case…
Part Number: LM5163-Q1 Other Parts Discussed in Thread: LMR38010-Q1 , Good morning
What is the maximum input leakage @150°C (or 125°C) of PGOOD port
(i.e. when voltage is regulated inside of the ‘good’ range , it should be a MOS --> Zero Gate Voltage…
Part Number: LM5163-Q1 Other Parts Discussed in Thread: LM5163 DC DC Converter-Ti.xlsx
Incase if the file is not accessible, please find the problem below
System Inputs
VIN = 16V to 32V
IOUT = 0.2A
VOUT = 12V
The system inputs are fed into…