Part Number: LM5164-Q1EVM Tool/software: Hello Everyone, Can you share the full bill of material for this LM5164-Q1EVM? The BOM's of all do not place components are not listed on the EVM user guide, that's why. With Regards.
Part Number: LM5164-Q1EVM Other Parts Discussed in Thread: LM5164-Q1 Hello, I just have ordered two 5164EVM board for testing. As is shown in Figure 3 in "LM5164-Q1 EVM User Guide", there are contact pins on positions of J1 , J4 and J5, respectively.…
Part Number: LM5164-Q1EVM Hi Team,
My customer requested an LM5164-Q1EVM EMC report based on CISPR 25 Class 5. Do we happen to have this? I found the EN 61326-1 test report but they requested CISPR 25 Class 5 specifically.
I wouldn't think we would…
Part Number: LM5164-Q1EVM Other Parts Discussed in Thread: LM5164-Q1 Dear Sir,
Can kindly share LM5164-Q1 EVM gerber file? my customer would refer it.
Thanks!
Steven
Part Number: LM5164-Q1EVM Other Parts Discussed in Thread: LM5164-Q1 , LM5146-Q1 hi Team,
our customer has a question that on the LM5164-Q1 EVM board
we see that the high/low side FET, Q1 and Q2. are two different part numbers with Q1 at 22mohm…
Part Number: LM5164-Q1EVM Other Parts Discussed in Thread: LM5164 Hello,
I am currently reading the LM5164-Q1EVM Datasheet and I see than the input voltage range Vin is from 15V to 100V.
However, given your component choices, the LM5164 should start…
Part Number: LM5169 Other Parts Discussed in Thread: LM5164-Q1EVM , LM5160 , LM5164 Hello Experts, My customer is evaluating LM5169 by replacing device of LM5164-Q1EVM. Customer has question as follows. Would you answer it, please? [Question] Customer…
Hi Siddharth,
Thank you for considering LM5164. You are looking for 12V and 1A regulated supply, why do you raise the output voltage to 20V?
Anyway, I am afraid the issue is related to your breadboard. The switching mode supplies should be implemented…
Hello Vaibhav
I guess the on-time is not enough to regulate the output voltage. The output voltage drops if the duty cycle is not increased enough when decreasing the input voltage. (Duty cycle =VOUT/VIN)
I recommend you to purchase https://www.ti…
Part Number: LM5164-Q1 Hi team,
Our customer tests our LM5164-Q1EVM, the input voltage is 60V(CH1), but the SW max voltage is 52V(CH2). Output voltage is 12V and load resistance is 50Ohms. Why SW voltage is lower than input voltage?