Part Number: LM5165 Other Parts Discussed in Thread: LM5161 , Hi
I have a power supply that requires a wide input voltage (14VDC to 50VDC) and a 12V output with a max current requirement of aoubout 50mA. The main requirement was extremely low Iq. I selected…
Part Number: LM5165 Dear,
I bought the IC chip of TI,LM5165YQDGSRQ1. At first, I thought it was a DIP type chip, but it was a very very small chip that needs soldering for use.
The datasheet of LM5165YQDGSRQ1 shows that package type of this chip is 'VSSOP…
Part Number: LM5165 Do i need to do Jitter test to validate buck converter?
What all are the basic tests to be conducted to do the validation of a VR.
Basically i do load regulation,efficiency , ripple and transient.
Is jitter test is required?
Any other…
Part Number: LM5165DESIGN-CALC Other Parts Discussed in Thread: LM5165 Hello, I could not locate the download link for the Design tool of LM5165. Please can you help by sharing download link.
https://www.ti.com/tool/LM5165DESIGN-CALC#overview
Part Number: LM5165LM5165Y has a fixed output of 3.3V due to the internal trimmed feedback resistor divider. I'd like to "trim" the output voltage of LM5165Yto 3.6V by a resistor added between Vout and FB. For this purpose I need to know…
Part Number: LM5165 Hi team,
My customer considers to use LM5165 and he would like to know state of PGOOD in case of EN=L.
Which state does PGOOD become L(GND) or Hi-Z when the device is disabled?
Best regards,
Shota Mago
Thanks. There are a lot capacitance added to the output of the 13V output rail. There is also a LM5165 flyback tied to 13V rail. What is the LM5165 working condition when the LLC starts to switch?
Please help get key signals scope picture.
Best Regards…
Part Number: LM5165
Dear,
I'm using the chip LM5165YQDGSTQ1 model, and designing the PCB with a guide of the datasheet.
In LM5165 datasheet, section 8.2.2 is showing the PFM converter at 3.3V, 50mA. Then I found that PGOOD, HYS, SS pins are not connected…
Part Number: LM5165 Hi team,
My customer wants to evaluate this device in the below application, Vin=15-51V, Vo=5V, Io=60mA; I use Webench to get below schematic, while my customer thinks the inductance value is too large for them, could you please help…
Part Number: LM5165 Other Parts Discussed in Thread: LMR36503
Good morning.....
I have been reading through the above subject datasheet and have a few questions/concerns:
My application is a high voltage from Li-Ion batteries (15-21V) to 3.3V. I will…