Part Number: LM5166 Other Parts Discussed in Thread: TIPD215 , DAC8775 , ADS8688 Hi everyone,
I am working on a power supply stage based on the TIPD215 reference design, which uses the LM5166 to generate a 12V rail from a 24V input.
In the TIPD215…
Part Number: LM5166
Hi team,
We are looking for a buck DC‑DC converter with a very low voltage drop in order to achieve behavior close to a pass‑through. Could you recommend some suitable products?
Input voltage: 5 V – 20 V
Output voltage: 5…
Part Number: LM5166 I am planning to use the LM5166YDRCR (PFM mode) with an input voltage range of 9.5 V to 32 V to generate a fixed 3.3 V output at 0.5 A .
While reviewing the datasheet, I noticed that under the Application and Implementation section…
Part Number: TPS54560B-Q1 Other Parts Discussed in Thread: TPS22990 , , LM5166 , LM74700-Q1
We're designing a rugged 12/24 V controller and use several TI parts in its power supplies: LM74700-Q1 (x3), LM5166, TPS54560B-Q1, TPS7B8233-Q1, TPS7A1650 and…
Part Number: LM5166 Tool/software: The LM5166DRCR is not outputting 5.0V as per the typical circuit schematic of the IC. The output is only about 1.28V. I have replaced the inductor, FB feedback resistor, SS capacitor, and RT resistor, but it still doesn…
Part Number: LM5166 Hello to everybody I have a LM5166 IC and I need to get 5V at its output. But I have 24V in SW pin and output, I don't know why!!!!
Part Number: LM5166 Hello,
As per the datasheet maximum low side current limit in COT Mode is 415mA , but maximum DC Load output current is 500mA.
If we consider ripple in inductor current to be around 30% of load , then low side current will…