Part Number: LM5168 Other Parts Discussed in Thread: LM5169 , Tool/software: We are currently designing a circuit using the LM5168 power IC and are utilizing the SNVR520 LM5169 Quick Start Calculator design tool. On the circuit diagram within the tool…
Part Number: LM5168 Other Parts Discussed in Thread: LM5169 , , LMR38015 I am designing with the LM5168PDDAR regulator and have been looking through the LM516x datasheet and have not been able to determine the efficiency of the LM516 8 PDDAR at low currents…
Part Number: LM5168 Tool/software: Hi,
I am using this IC for my project,
Requirement is : 10V output voltage and 300 mA current.
1) Input voltage range mentioned in datasheet as 6V to 115V, while in simulation I am not getting output up to 19V…
Part Number: LM5168 Tool/software: Dear team,
I used LM5168 output 5V, when loaded, the inductor will make a whistling sound.
Can you help me see what improvement methods are available?
The circuit diagram is as follows:
Part Number: LM5168-Q1 Other Parts Discussed in Thread: LM5168PEVM Hi Due to problems with sleep functionality of LM5168P I'm asking for rewiev of board design. Problems with converter are described in different thread: https://e2e.ti.com/support/power…
Part Number: LM5168 Tool/software: Hello,
We have used the LM5168 regulator on our board. This regulator is supposed to take an input voltage between 75V and 48V (connected to an 18S battery). We aim to have two 3.3V outputs for two different circuits…
Part Number: LM5168
Tool/software:
Is it possible to simulate a LM5168P design in Webench?
Please provide a link or explain how to do this.
When I attempt to simulate LM5168P it uses LM5168F. These parts behave differently.
Part Number: LM5168-Q1
Hi
I've made a design of LM5168P converter for 19-62V input voltage, 10V 50mA output. Quite standard design, made 9pcs. of prototype boards and after tests they were working ok. On low loads "sleep" function (sometimes called…
Part Number: LM5168 Hello,
We are considering using the part LM5168FDDAR, package number DDA(HSOIC,8).
We have reviewed the datasheet, revision SNVSBS7B, published DECEMBER 2021 REVISED DECEMBER 2024. Pages 47 onwards show the dimensions for DDA(R…
Part Number: LM5168
Tool/software:
Hi support all.
The LM5168 seems to be able to generate -80V from 24V, but the output current cannot achieve 130mA.
Can you suggest a product that can meet this requirement?
An additional requirement is that…