Part Number: LM5168-Q1 Other Parts Discussed in Thread: LM5168PEVM Hi Due to problems with sleep functionality of LM5168P I'm asking for rewiev of board design. Problems with converter are described in different thread: https://e2e.ti.com/support/power…
Part Number: LM5168-Q1 Tool/software: Hi expert,
My customer is looking for a suitable DCDC/ LDO to meet below request, do you think LM5168-Q1 is most suitable device for customer or do we have cheaper device than LM5168-Q1?
VIN: 48V (MAX VIN >…
Part Number: LM5168-Q1
Hi
I've made a design of LM5168P converter for 19-62V input voltage, 10V 50mA output. Quite standard design, made 9pcs. of prototype boards and after tests they were working ok. On low loads "sleep" function (sometimes called…
Part Number: LM5168-Q1 Two times 5V are needed with one being isolated. For single output I could use 68 uH TYS6045680M or similar.
I'm not familiar with FlyBack transfomers. Which specific part is recommended in this case to replace the simple inductor…
Part Number: LM5168-Q1 Other Parts Discussed in Thread: LM5168 , LM5017 , LM5117 Tool/software: My customer is using LM5168 to build the fly-buck circuit.
300K frequency; IOUT1=12mA,IOUT1=140mA, input voltage VIN=24V,VOUT1=VOUT2=5V
According to…
Part Number: LM5168-Q1 Tool/software: Hey all,
I've got a peculiar situation here. The output of this buck is set to 6V through the feedback resistors, but I need to have 8.2V on the output temporarily for One Time Programable programming during production…
Part Number: LM5168-Q1 Other Parts Discussed in Thread: LM5168 Hi,
Right now we are using LM5168 IC for some applications.
We need calculator for calculating ripple circuit parameters and some another parameters.
The calculator is not available…
Part Number: LM5168-Q1 Other Parts Discussed in Thread: LM5168 Tool/software: Hello,
We have developed a PCB using LM5168 regulator in buck mode to supply our chip at 1.8V (~100mA).
In the lab, there is output voltage freeze at 0.8V when power up…
Part Number: LM5168-Q1 Hello E2E,
e2e.ti.com/.../3877515
I'm coworker with Kengo. Kengo has not to received reply mail about RTM schedule. Can I have information about RTM schedule?
Regards, ACGUY