Part Number: LM5169 Tool/software: I received an encrypted TI file for the LM5169 model to use in PSpice simulations. However, I discovered that this model requires version 17.4 or later to function properly. The PSpice executable I obtained via a TI…
Part Number: LM5169 Tool/software: I am designing a fly-buck circuit with
Primary side
Sec side
Vout=5V Iout=250mA Ripple 25mV
Vout=5V Iout=1-3mA (75mA pulse or max for some time) Ripple 25mV
However, during…
Part Number: LM5169 I have designed a PCB layout using LM5169PDDAR, and tried to keep the high current switching loop as short as possible. Can someone review my PCB layout so that we should not face any issue in standards like IEC 55025/ CISPR 25 for…
Part Number: LM5169 I want to use the LM5169 to generate a app. 7V primary output with a current consumption going from almost no load (< 0,1mA) to 300mA. The isolated secondary side should be 12V with a load going from no load to a few mAs.
Is this…
Part Number: LM5169 Tool/software: Hi,
In my application I use Type 3 schematic for minimum ripple for an application of 115V input and output of 5V, 0.6A max:
with L0= 100uH, 1 A saturation current, Ra = 178k, Ca=3300pF, Cb=56pF, Rt = 49.9k,…
Part Number: LM5169 Tool/software: hi.
It's a circuit using 48V to 12V using LM5169, but I keep getting the problem of dying. The 48V is buried with the motor power end and has 5 10uF bypass caps. The 12V output terminal is in use for internal power…
Part Number: LM5169 Tool/software: The system input is 80V-100V, and the output is 24V. How to protect the input? Could you please recommend the protection scheme or materials?
Part Number: LM5169 Tool/software: Hi team,
I have question about the maximum output voltage it can achieve. Could you please help confirm this parameter. Thank you.
Thanks
Lillian