Hi EM,
Thank you so much for your support.
Please this internal platform link: https://e2e.ti.com/support/power-management-group/power-management---internal/f/power-management---internal-forum/1245039/lm5170-q1-lm5170-q1-spice-module-confirmation
Part Number: LM5170-Q1 Other Parts Discussed in Thread: TIDA-01168 , LM5170EVM-BIDIR Hello,
Can we achieve required configuration using 2 Phase buck by using LM5170-Q1? and can we increase the power upto 5KW by using multiphase (6 Phase)?
Can TI provide…
Part Number: LM5170-Q1 Other Parts Discussed in Thread: LM5170 Hello,
I am working on a high-power Buck Converter. The specs are as follow:
Vin: 40V ~ 60V
Vo: 24V
Io = 50 A
# of phases = 2
fsw = 80 kHz
Control Mode: Output Voltage Control Mode
Mode of…
Part Number: LM5170-Q1 Could you please give me advice for LM5170-Q1?
As attached file, the system shows IPK may affect by the RAMP and duty. But calculator doesn't change Boost/ Buck mode duty cycle when %. RAMP selection is updated. 1. Let me know…
Part Number: LM5170-Q1 Other Parts Discussed in Thread: LM5170 Can we do following things with LM5170 Current controller IC
1) Resistor less current sense like Inductor DCR to measure Inductor current is possible ?
2) maximum how many phase connections…
Part Number: LM5170-Q1 Other Parts Discussed in Thread: LMG1205 , LM5170 I want to use external gate driver LMG1205 with LM5170 for developing GaN based bidirectional converter. Please help us with necessary wiring diagram.
Other Parts Discussed in Thread: LM5176-Q1 Hi Brigitte,
Thanks a lot for your suggestion.
And what is the max output current of LM5176-q1? I can't find it in the DS. Is it depend on the MOS they use?
Best Regards,
Brian
Part Number: LM5170-Q1 Other Parts Discussed in Thread: LM5170EVM-BIDIR Hello,
I have a question that I need this boost converter EVM module with 24V input. This 12V input port can be connected to 24V battery?
And the duty cycle is varying in this module…
Part Number: LM5170-Q1 Hi, I have a question regarding EVM of boost converter. Can I take the signal from that and apply to a microcontroller outside for another application?
Please also note that the LM5170 model is modified to work on single channel with constant current mode (set by ISETA), which was tested to work fine. The modification of the driver part (replacement of MOSFET by GaN) is done on that.