Part Number: LM5170EVM-BIDIR Tool/software: Hello, if I want to use Boost mode by connecting a 12V, 10A power supply on the LV side and connecting a 20ohm resistor on the HV side, I have a question: Is the 10A current rating of the power supply sufficient…
Part Number: LM5170EVM-BIDIR Other Parts Discussed in Thread: LM5171 , LM5170
Tool/software:
Hello
I am studying the operation of the LM5170-Q board in Boost mode. I have closed the pins according to the manual and have shorted the 2 pad breakers on the…
Thank you for your answer.
Today, I tested using an input voltage of 12V/10A and H V side connecting with R = 200 Kilo-ohms. However, the output voltage on the HV side was only around 24-25V. Is there anything problem? Thank you. Best Regards
Part Number: LM5170EVM-BIDIR Other Parts Discussed in Thread: LM5171 , LM5177 , LM51772 , LM5170 Trying to make a MPPT algorithm where low side its 12 V and highside should be 48. My main concern is with the DC-DC conveter. Is LM5170EVM-BIDIR suitable for…
Part Number: LM5170EVM-BIDIR Other Parts Discussed in Thread: LM5170 , LM5171EVM-BIDIR Hello! I want to make a 12/24 V bidirectional power converter (with the LM5170 EVM) using the F28379D Launchpad as MCU. In the user's guide it says to contact TI for…
Part Number: LM5170EVM-BIDIR Hi,
We need help to achieve following operating conditions. Also referred EVM user guide but not getting expected results.
Mode : Boost mode
Input voltage : 12VDC
Output voltage: 48VDC
Output wattage: 700W
1. Can you please…
Part Number: LM5170EVM-BIDIR Hello
I have a query related to power supply at 3.3V, If I did not install resistor R4 and I need to start the board through power supply at 3.3V, How much current setting should I need for a board at this pin?
Thanks
Part Number: LM5170EVM-BIDIR Other Parts Discussed in Thread: LM5170 Hello
I have some confusions in connecting two EVM's for three phase Boost confuguraiton.
1. For the second board, do I also need the same jumpers setting?
2. If for example for testing…
Part Number: LM5170EVM-BIDIR Hello
I have some confusion regarding output voltage control:
1. If I am using MCU for output voltage control then do I need to adjust R77? If yes then how?
2. If I am using on-board voltage contol without MCU then how I can…
Part Number: LM5170EVM-BIDIR I am using LM5170EVM-BIDIR as a controlled buck converter, and I am looking for a way to sense the inductor current. Could you please suggest any methods or approaches for sensing the inductor current?
Regards,
Gaureej