Part Number: LM5175-Q1 Other Parts Discussed in Thread: LM5176-Q1 , , LM5175 , LM5176 Hello team,
Could you help provide a comparison table between LM5175-Q1 and LM5176-Q1?
Thank you so much.
Best regards,
Lanxi Li
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5175 , LM5176 Hello! I am comparing the LM5175 with its successor the LM5176. I would like to know a few things: What does it mean that the Vin is 2.5V with bias for the LM5176? Can Vin go as low…
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: LM5175-Q1 Tool/software: Hi, Could you please help me to perform simulation for traction inverter. It will beneficial for me to validate design. I am using UCC14240, UCC5880QDFCRQ1,LM5175-Q1.
I will…
Part Number: LM5175-Q1 Hello, I am currently testing a design using the LM5175-Q1 with a 6.5-32V input and 24V 12A output. All component values were derived from the QuickStart tool. The circuit was working as intended over the full range of input voltages…
Part Number: LM5175-Q1 Hello, my team has been working on integrating the LM5175-Q1 buck-boost into our design. We have an input voltage ranging from 6.5 - 32V, and a 24V output at 12.5 A peak current. We have been attempting to simulate this circuit…
Part Number: LM5175-Q1 Design parameters used are VIN 6V-36V, VOUT 12.00V @ 15A. I did not c ustomize the default design that was generated.
PDF Print Report (attached) exports with no issue, but selecting "Cadence OrCAD" and attempting to "Export Design…
Part Number: LM5085-Q1 Other Parts Discussed in Thread: LM5085 , LM5175 Tool/software: I want to use the LM5085 in the to genrate the 7.5V, 5A.
But VIN is 4.5V -36V, so I have the question, when the VIN is less than the VOUT, maybe VIN is 4.5V to 7.5V. …
Part Number: LM5175-Q1 Other Parts Discussed in Thread: LM5175 , Tool/software: WEBENCH® Design Tools Hi,
We are trying to use LM5175-Q1 as a programmable constant current source with output current selectable 0-20 A. The LM5175 Rsns is used to limit output…
Part Number: LM5175-Q1 Other Parts Discussed in Thread: TPS65131 Hi,
I need to design a buck-boost voltage regulator circuit with below specification:
Vin (min)=8V
Vin (max)=38V
Vout= 24V
Iout= 7A
I used TI WEBENCH for the design and simulation. Attaching…
Part Number: LM5175-Q1 Other Parts Discussed in Thread: LM5175EVM , LM5175 Hi Experts,
We want to modify LM5175EVM to support min Vin 3.5V. How can we do that?
Regards,
Uchikoshi