Part Number: LM5175EVM-HP Other Parts Discussed in Thread: LM5175 , LM51770 , LM51772
Hi TI team
I'm currently bench-testing the LM5175EVM-HP evaluation board, and I have an observation regarding the boost-side bootstrap capacitor charging mechanism…
Part Number: LM5175EVM Other Parts Discussed in Thread: LM5175 Hello Experts, We actually require IBIS file format of IC LM5175 for our simulation, if you can provide the IBIS file of the IC it will be very helpfull. Thank You, Shivam Mehar ARAI-Indi…
Part Number: LM5175EVM Hi Expert
as below discussion, VIN=11.3V~11.7V, 12.4V~12.8V, 14.3V~15V the reason for the signal not consist that the value of Cslope.
LM5175EVM: gate driver signal not consist - Power management forum - Power management - TI…
Part Number: LM5175EVM-HD Other Parts Discussed in Thread: LM5175 I want to limit the output current of the LM5175 integrated circuit. When it reaches 11A, the system should automatically shut down. How can I achieve this?
Part Number: LM5175EVM-HP Other Parts Discussed in Thread: LM5175 Hi
we need to boost 5v to 12V 12 AMP, whether this EVM support for 5V input
can I use this EVM for 5V input?
(The LM5175 is a synchronous 4-switch buck-boost controller capable of…
Part Number: LM5175EVM Hi, team
my customer are testing LM5175EVM, have have questions below. (LGS1: high side, LGS2: low side)
1.VIN=14.3V~15V,VOUT=12V/IO=6A, at transition to BUCK, the output not stable, the waveform shows below
2.VIN=11.3V…
Part Number: LM5175EVM-HP Other Parts Discussed in Thread: LM5175QUICKSTART-CALC , LM5175 , LM5177 , LM5122 Hi there,
we are using the LM5175EVM-HP evaluation board for 12V output but now we would like to switch the output to be 18V. L ooking at LM5175EVM…
Part Number: LM5175EVM Other Parts Discussed in Thread: LM5176 Dear Sir,
I have some question for LM5175EVM as attached file.
1. Why it use D1, D2 for reference design. could you explain usage of D1, D2 as below picture.
I think it seems free…
Part Number: LM5175EVM-HP Hi
We would like to use the LM5175EVM-HP to run the validation for the application (12V/15A). However, we were seeing the switching PWW rising issue and would like to check with you.
We know the LM5175EVM-HP can only support…