Part Number: LM5175EVM Other Parts Discussed in Thread: LM5175 Hi,
I use LM5175 for a reference design for 12~19Vin and 12Vout
But I got an issue for IC controller broken at switch on off test and short protection.
Is that I don't use 8.2V ZD at…
Part Number: LM5175EVM-HP Hello I am attempting to make a battery charger based off the TI LM5175EVM-HP board. I am attempting to use this so I can charge a 12V lead acid battery off a variable input. My power source is going to be variable but capable…
Part Number: LM5175EVM Other Parts Discussed in Thread: LM5175 , LM2775 Hi ,
I am using LM5175 EVM SV601130B - My input voltage range is 3.7V to 4.3V. I have changed the enable resistor divider resistor R16 to 143K and R13 is 249K - this should allow…
Part Number: LM5175 Hi,
I'm testing the LM5175, using LM5175EVM board with an input 12.5V, suppling a PC card with a stress test that is working.
I don't exactly which is load profile that the tool generate but I didn't detect too much high peaks…
Part Number: LM5175EVM Other Parts Discussed in Thread: LM5175 , LM5176 , LM5175RHFEVM-HD Hello
I am using LM5175 to generate 12 V and 6 A output .
The input voltage range is 20- 34 V which is obtaining through step down tansformer and Full wave Bridge…
Part Number: LM5175EVM-HP Other Parts Discussed in Thread: LM5175EVM , LM5176 Tool/software: WEBENCH® Design Tools I checked the LM5175EVM Inductor temperature when Vin24V and Vin36V both no load.
why the L1(chock) temperature is too high different…
Part Number: LM5175EVM-HD Hi Sir, I looks LM5175EVM-HD layout guide, but have some question need you help. How to do design different diameter of via for current flow? and how to calculate it?
Part Number: LM5175EVM-HD Hi,
The minimum input voltage of LM5175EVM-HD is mentioned such as following.
My customer is requesting to work this EVM from 4V.
I think that EV/UVLO divider shoud be changed.
Should they change FETs and inductor?…