Part Number: LM5175EVM Other Parts Discussed in Thread: LM5175 , LM5176 , LM5175RHFEVM-HD Hello
I am using LM5175 to generate 12 V and 6 A output .
The input voltage range is 20- 34 V which is obtaining through step down tansformer and Full wave Bridge…
I assume the system blocks upload of .xlsm file type.
Please check if below can help.
C:\Users\nx024387\Downloads\LM51772_Buck-Boost_Quickstart_Tool_V1_2_0_1
or
LM51772_Buck-Boost_Quickstart_Tool_V1_2_0_2.xlsx
Other Parts Discussed in Thread: LM5175EVM , LM5175 , LM5175RHFEVM-HD Hi All
I have built a power supply using LM5175 using the reference schematic of LM5175EVM.The required output voltage is 12v at 5A. The schematic is attached below. All the components…
Part Number: LM5176 Two circuits designed using the TI LM5176:
a. Input 9~36V, output 20V 8A;
b. Input 9~36V, output 24V 8A;
Please assist in confirming whether there are any problems with the design. POWER_THOR_12_24V.pdf LM5176_Buck-Boost_Quickstart_Tool_V1_0_2_9…
Hi Stefan,
Thank you very much for your reply.
I attached the calculator. I changed the original extension, xlsm to xls because xlsm file can not be attached. So please change the file extension from xls to xlsm when you open the file.
And could…
Hi Youhao,
Thank you for your reply.
I understand if CSLOPE is too small, duty cycle may become large.
Could I confirm your comment.
You mention 82pF and 150pF, which value is suitable of the customer's application.
According to the excel calculation…
LM5177 Buck-Boost Quickstart Tool V1_1_2.xlsx FAUL0530-1R2MTpdf.pdf FAUL1050-2R2MT.pdf 华润微-CRSM023N04N2Z draft-MOSFET.pdf
Hi Stefan,
The design requirement:
1) Input normal 12V, Output: adjust from 6@7A to 18V@8A, normal 16V@10A.
2) Input normal…