Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 , Hi TI Expert,
LM5176 schematic as below, Vin=9~32V, Vout=16V.
A sample part returned from the factory shows this phenomenon. With Vin=12V and a light load (around 0.17A) during cold…
Part Number: LM5176 Other Parts Discussed in Thread: LM5175 , , I replace LM5175 by LM5176 on the same board. the schématic is here : schematic_LM5176.pdf The efficiency for the LM5175 is 97% for Vin=16V, Vout=12V 4A. I change the LM5175 by the LM5176…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 , LMZM33606 Can the LM5176-Q1 to convert as an inverting buck-boost converters to produce negative voltage output? If yes, could you provide reference design of it.
Part Number: LM5176 Using Webench design tool I have made a 24V Buck-Boost converter with Vin 22-50V. It seems that both of the external mosfets are switching allways no matter if the converter should be in Boost, Buck or Buck-Boost mode, though the duty…
Part Number: LM5176 Two circuits designed using the TI LM5176:
a. Input 9~36V, output 20V 8A;
b. Input 9~36V, output 24V 8A;
Please assist in confirming whether there are any problems with the design. POWER_THOR_12_24V.pdf LM5176_Buck-Boost_Quickstart_Tool_V1_0_2_9…
Part Number: LM5176 Hello, our team is designing a DC power supply consisting of the LM5176. The quickstart excel tool was used for component selection. Our DC power coming in is roughly 35-36vdc. We are attempting to vary the output voltage between 0…
Part Number: LM5176 Other Parts Discussed in Thread: UCC29002 , , LM51770 , LM51772 Hi TI Team,
Is LM5176+UCC29002 feasible? Are there any risks? follow as. Thanks.
Part Number: LM5176 Hi,
At present, the following analysis and processing have been carried out on the damaged chip LM5176PWPR:
1. The fourth pin (MODE) of the LM5176PWPR chip on the damaged motherboard was measured tohave a voltage
of only 3…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 , LM51770 , LM51772
Is the LM5176-Q1 a true bidirectional buck-boost converter capable of transferring power from VOUT back to VIN?
The datasheet mentions that the inductor current can…
Part Number: LM5176 Hi,
LM5176 used for 12V to 12V system, the output current is more than 20A(above 200W output), and then, we find LM5176 is failure and the impedance of the BOOT1 is abnormal, we modify the inductor to 1uH but there are about 2-3W…