Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176EVM-HP , LM5176 Hi Expert,
Hope you have a nice day!
About LM5176-Q1, if we want to improve the output current, can we parallel the MOSFETs + inductor part?
Thanks!
Best Regards…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 , LM51770 , LM51772
distribution to downstream boards.
Parameter
Requirement
Input Voltage Range
9V to 32V DC
…
Part Number: LM5176-Q1 Tool/software: Dear TI,
We have query for below circuit. Kindly confirm VISNS capacitor C value.
we are using C 150pF/50V at VISNS pin . input 8V to 24VDC, 38V 400ms load dump pulse.
output : 36V, 1000mA or 800mA LED Load…
Part Number: LM5176-Q1 My design requirements are Vin- 6 to 36V; Vout-7.5V; Iout-5.2A.Is this IC is suitable for this application? I tried to simulate same in webbench but it is showing following error
Design update failed. OpVal table param temperature…
Part Number: LM5176-Q1 Tool/software: Hi,
We are considering the LM5176-Q1 for a step-up (boost-only) converter :
Vin : 10-16V
Vout : 42V
Iout : 10A max (420W)
The constant-current voltage foldback trick (snva846) would be very useful for battery…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 Tool/software: Hi all,
In the LM5176-Q1 there is overcurrent protection. It senses the voltage across CS/CSG.
In our design this is used in combination with hiccup mode.
We have verified…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 , LM51772 Tool/software: Customer is finding a Buck-boost solution, could you pls help advise? Thanks.
input:10-40VDC
output:24V or 28V/ 30A (there are two project, one is 24V output,…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 Tool/software: The leakage at PGOOD is 0.1mA, which is significant when it's about reducing the standby. Knowing this is a worst case value, please give a supporting graph to estimate the…
Part Number: LM5176-Q1 Tool/software: Hello TI support team,
We noticed on data sheet for TIPN LM5176-Q1 that you use chlorine based flame retardant. Could you explain how this retardant works in a case when the component gets exposed to high temperatures…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: TL431-Q1 , Tool/software: Hello, I am using the LM5176-Q1 buck-boost regulator with the output charging up a 12V supercapacitor bank, where the supercapacitors are 5 in series each with a TL431-Q1…