Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 Hi, Sir,
Now I encounter an issue when I use LM5176 working at the boost mode and then hope to get 15.5v output voltage when the input voltage is 12v, i.e. the firstly HDRV1 MOSFET can't be…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 , LM5177 , LM5175 , Hi Team,
I am currently using the LM5186-Q1, but due to the recent shortage of semiconductors,
I would like to use it exclusively for step-down in order to reduce the number…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 , CSD17573Q5B , CSD18532Q5B Hello,
I have designed a power management board based on LM5176 evaluation board circuit including same BOM, but after receiving the samples and test the board unfortunately…
Hi Stefan,
The customer has new discovery. In their board, there are two LM5176-Q1, one LM5176-Q1 powers SOC1, and another powers SOC2. These two LM5176-Q1's schematics are identical, and these two devices' load are also same. Currently the load is…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 , CSD17573Q5B , CSD18532Q5B Hello,
I have designed a power management board based on LM5176 evaluation board circuit including same BOM, but after receiving the samples and test the board unfortunately…
Part Number: LM5175-Q1 Other Parts Discussed in Thread: LM5176-Q1 , , LM5175 , LM5176 Hello team,
Could you help provide a comparison table between LM5175-Q1 and LM5176-Q1?
Thank you so much.
Best regards,
Lanxi Li
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 We are still seeing issues with the inductor getting hot.
We use the same design to generate 2 different voltages. They are both boost configurations. One has 24V in and 30V out. The other…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5175 , LM5176 Hello! I am comparing the LM5175 with its successor the LM5176. I would like to know a few things: What does it mean that the Vin is 2.5V with bias for the LM5176? Can Vin go as low…
Part Number: LM5176-Q1 We have an existing design which generates 30V from 24V input with the LM5176-Q1. We have received a new batch of assemblies which are exhibiting issues. The issue is that the Inductor get extremely hot. The last build of boards…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 Hi TI Team,
Can you explain how to calculate power dissipation of LM5176QPWPRQ1 buck boost IC.