Part Number: LM51772EVM-HP Other Parts Discussed in Thread: LM51772 Hello,
the evaluation module for the LM51772 includes footprints which provide the option to populate addional MOSFETS for parallel operation to Q1 and Q3.
I was wondering: when would…
Part Number: LM51772EVM-HP Other Parts Discussed in Thread: LM51772 , PMP23377 , , LM5177 Hello expert,
May I ask can we refere to the reference design, PMP23377 to power 200W load with using LM51772 as well? Can LM51772 be also used to drive GaN FET…
Part Number: LM51772EVM-HP Tool/software: Are the schematic and/or layout files available for this board ? This uses the
LM51772RHAR
55V wide VIN four-switch buck-boost controller with I2C interface that has
a 55V max on both Vin and Vout using…
Part Number: LM51772EVM-HP Other Parts Discussed in Thread: LM51772
Tool/software:
LM51772 EVM Board Setup
Left side: power supply
Right side: Battery
To force a current flow from right to left, the output voltage of the LM51772…
Part Number: LM51772EVM-HP Tool/software: I am using LM51772EVM-HP to debug the constant current function and need to adjust the current through I2C. However, I found that the current is always limited to 5.4A in the constant current state. I tried to…
Part Number: LM51772EVM-HP Other Parts Discussed in Thread: LM51772 Tool/software: Hi Team,
I am using GUI with LM51772EVM. I would like to change the Vout in real time by GUI. In addition to adjust the scroll bar, do we need to issue any other part…
Part Number: LM51772EVM-HP
Tool/software:
Greetings,
I'm using the LM51772EVM-HP evaluation board and seek to control the output voltage - I connected AGND and SLOPE on the board in order to use the I2C interface. I can successfully read and write…
Part Number: LM51772EVM-HP Other Parts Discussed in Thread: USB2ANY Tool/software: I currently studied the LM51772EVM and want to apply on our design products.
The board is OK connect to I2C and change the setting with USB2ANY on GUI interface,
however…
Part Number: LM51772EVM-HP Other Parts Discussed in Thread: LM51772 Tool/software: Salutations,
I'm currently working with the LM51772 Evaluation board and operate it using I²C - I merely read registers and write to the V_OUT registers, I have however…