Part Number: LM5185-Q1 Tool/software: Hello TI team,
I have designed and prototyped an isolated DC-DC converter using the LM5185QPWPRQ1. The design converts a 24-27V DC input to two isolated 15VDC outputs. Each output is rated for 7.5W, and during our…
Part Number: LM5185-Q1 Other Parts Discussed in Thread: LM5185
Tool/software:
Team,
Specs are below :
Vin : 9V - 32V, Vout :15V, load : 0.5A
Vout is dropping at different intervals without resistor load and with resistor load.
Additionally, with increasing…
Part Number: LM5185-Q1 Other Parts Discussed in Thread: LM5185 Hello,
Is you try LM5185 with Orcad Pspice in an example because me it doesn't work wit the model given by the evaluation module?
Cordially
Biellmann Cedrick
Part Number: LM5185-Q1 Other Parts Discussed in Thread: LM5185
Tool/software:
Hi Team,
Finally, I have created the schematic 125W Iow cost Isolation design using LM5185PWPR IC. Thanks for Youhao, Eric lee and David suggestions and supports.
I got support…
Part Number: LM5185-Q1 Hi TI,
User guide: https://www.ti.com/lit/ug/snvu869/snvu869.pdf?ts=1711677902689&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FLM5185EVM-SIO%253FkeyMatch%253DLM5185-Q1+SINGLE-ISOLATED
Customer can`t search the ZD2250-AE…
Part Number: LM5185-Q1 Other Parts Discussed in Thread: LM5185 Hello, please consult our input voltage 4-40V, we want to output voltage 12V, current 1A, can we use the LM5185-Q1 chip to achieve? thank you.
Part Number: LM25184-Q1 Other Parts Discussed in Thread: LM5185-Q1 , Tool/software: Hello,
I am using input 8V to 16V. My desired output is 14V/ 16V with 2.5A output current. Can I use this device?
Part Number: LM5180-Q1 Other Parts Discussed in Thread: LM5180 , LM5185-Q1 , LM5185 Tool/software: Hi TI Team,
I am currently facing Radiated Emission (RE) issues (EN 55032, CLASS B target) with a flyback design using the LT3758. I am looking for a low…
Part Number: LM5185 Other Parts Discussed in Thread: PSPICE-FOR-TI , , Tool/software: I have installed PSPICE-FOR-TI in order to run simulations for the LM5185, but I am having issues. The simulations run, but the gate drive remains low after the soft…
Part Number: LM5180-Q1 Other Parts Discussed in Thread: LM25180 , LM5180 , LM5185 Tool/software: Hi sir,
I want to design power supply using LM5180-Q1 IC which will have 2 outputs say 5 Volt 500 mA each. Can you suggest suitable fly-back transformer…